AfuMathOperationOuterInterpolation Enumeration

NXOpen.CAE.AfuMathOperation.OuterInterpolation is an alias for NXOpen.CAE.AfuMathOperationOuterInterpolation

class NXOpen.CAE.AfuMathOperationOuterInterpolation

Bases: object

Defines the outer interpolation method

Enum Members

Enum Member Enum Member Description
Zero
Interpolates values with zero
Curve
Interpolates values with curve points
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.