ThicknessBuilderEntityType Enumeration

NXOpen.CAE.ThicknessBuilder.EntityType is an alias for NXOpen.CAE.ThicknessBuilderEntityType

class NXOpen.CAE.ThicknessBuilderEntityType

Bases: object

Option to Info on Node or Element

Enum Members

Enum Member Enum Member Description
Node
Info on node
Element
Info on element
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.