ModelUpdateOptimOptionsBuilderSteepestDescMethodChoice Enumeration

NXOpen.CAE.ModelUpdateOptimOptionsBuilder.SteepestDescMethodChoice is an alias for NXOpen.CAE.ModelUpdateOptimOptionsBuilderSteepestDescMethodChoice

class NXOpen.CAE.ModelUpdateOptimOptionsBuilderSteepestDescMethodChoice

Bases: object

the mode of the Steepest Descent method

Enum Members

Enum Member Enum Member Description
Linear
Linear mode
Fractional
Fractional mode
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.