MMCCreateBuilderMeshMatingType Enumeration

NXOpen.CAE.MMCCreateBuilder.MeshMatingType is an alias for NXOpen.CAE.MMCCreateBuilderMeshMatingType

class NXOpen.CAE.MMCCreateBuilderMeshMatingType

Bases: object

Types of Mesh Mating Conditions

Enum Members

Enum Member Enum Member Description
GlueCoincident
glue coincident
GlueNonCoincident
glue non-coincident
FreeCoincident
free coincident
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.