ClippingParameters Class¶
-
class
NXOpen.CAE.
ClippingParameters
¶ Bases:
NXOpen.TaggedObject
This class is worked as a packet of information that can be used to set the clipping parameters of a
NXOpen.CAE.Post
object.<br/>Use
NXOpen.CAE.ResultManager
to create anNXOpen.CAE.ResultParameters
<br/>You can modifiy these values but validation of correctness will only be perfomed when this object is set to a
NXOpen.CAE.Post
objectTo obtain an instance of this class use
NXOpen.Session.ResultManager()
.New in version NX7.5.1.
Methods¶
Method | Description |
---|---|
GetClipValue | Ask clip value @return |
GetCoordinateSystem | Ask coordinate system @return |
GetPlane | Ask plane @return |
GetSelectedCoordinateSystem | Ask selected coordinate system |
GetShowClippedGhost | Ask show clipped ghost @return |
GetShowOutline | Ask show outline @return |
GetSide | Ask side @return |
SetClipValue | Set clip value |
SetCoordinateSystem | Set coordinate system |
SetPlane | Set plane |
SetSelectedCoordinateSystem | Set selected coordinate system |
SetShowClippedGhost | Set show clipped ghost |
SetShowOutline | Set show outline |
SetSide | Set side |
Method Detail¶
GetClipValue¶
-
ClippingParameters.
GetClipValue
¶ Ask clip value
Signature
GetClipValue()
Returns: Return type: float New in version NX7.5.1.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
GetCoordinateSystem¶
-
ClippingParameters.
GetCoordinateSystem
¶ Ask coordinate system
Signature
GetCoordinateSystem()
Returns: Return type: NXOpen.CAE.ResultCoordinateSystem
New in version NX7.5.1.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
GetPlane¶
-
ClippingParameters.
GetPlane
¶ Ask plane
Signature
GetPlane()
Returns: Return type: NXOpen.CAE.PostClipPlane
New in version NX7.5.1.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
GetSelectedCoordinateSystem¶
-
ClippingParameters.
GetSelectedCoordinateSystem
¶ Ask selected coordinate system
Signature
GetSelectedCoordinateSystem()
Returns: a tuple Return type: A tuple consisting of (source, id). source is a NXOpen.CAE.ResultCoordinateSystemSource
. id is a int.New in version NX7.5.1.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
GetShowClippedGhost¶
-
ClippingParameters.
GetShowClippedGhost
¶ Ask show clipped ghost
Signature
GetShowClippedGhost()
Returns: Return type: bool New in version NX7.5.1.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
GetShowOutline¶
-
ClippingParameters.
GetShowOutline
¶ Ask show outline
Signature
GetShowOutline()
Returns: Return type: bool New in version NX7.5.1.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
GetSide¶
-
ClippingParameters.
GetSide
¶ Ask side
Signature
GetSide()
Returns: Return type: NXOpen.CAE.PostClipSide
New in version NX7.5.1.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
SetClipValue¶
-
ClippingParameters.
SetClipValue
¶ Set clip value
Signature
SetClipValue(clipValue)
Parameters: clipValue (float) – New in version NX7.5.1.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
SetCoordinateSystem¶
-
ClippingParameters.
SetCoordinateSystem
¶ Set coordinate system
Signature
SetCoordinateSystem(coordinateSystem)
Parameters: coordinateSystem ( NXOpen.CAE.ResultCoordinateSystem
) –New in version NX7.5.1.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
SetPlane¶
-
ClippingParameters.
SetPlane
¶ Set plane
Signature
SetPlane(plane)
Parameters: plane ( NXOpen.CAE.PostClipPlane
) –New in version NX7.5.1.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
SetSelectedCoordinateSystem¶
-
ClippingParameters.
SetSelectedCoordinateSystem
¶ Set selected coordinate system
Signature
SetSelectedCoordinateSystem(source, id)
Parameters: - source (
NXOpen.CAE.ResultCoordinateSystemSource
) – - id (int) –
New in version NX7.5.1.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
- source (
SetShowClippedGhost¶
-
ClippingParameters.
SetShowClippedGhost
¶ Set show clipped ghost
Signature
SetShowClippedGhost(showClippedGhost)
Parameters: showClippedGhost (bool) – New in version NX7.5.1.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
SetShowOutline¶
-
ClippingParameters.
SetShowOutline
¶ Set show outline
Signature
SetShowOutline(showOutline)
Parameters: showOutline (bool) – New in version NX7.5.1.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
SetSide¶
-
ClippingParameters.
SetSide
¶ Set side
Signature
SetSide(side)
Parameters: side ( NXOpen.CAE.PostClipSide
) –New in version NX7.5.1.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)