DurabilityStrainGageAnalyzerBuilderGageSourceEnum Enumeration

NXOpen.CAE.DurabilityStrainGageAnalyzerBuilder.GageSourceEnum is an alias for NXOpen.CAE.DurabilityStrainGageAnalyzerBuilderGageSourceEnum

class NXOpen.CAE.DurabilityStrainGageAnalyzerBuilderGageSourceEnum

Bases: object

the gage source enum.

Enum Members

Enum Member Enum Member Description
Response
Response
Afu
Afu
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.