BeamEADBuilderVectorChoiceType Enumeration

NXOpen.CAE.BeamEADBuilder.VectorChoiceType is an alias for NXOpen.CAE.BeamEADBuilderVectorChoiceType

class NXOpen.CAE.BeamEADBuilderVectorChoiceType

Bases: object

indicates which vector choice to use

Enum Members

Enum Member Enum Member Description
Horizontal
the vector is defined to be horizontal
Vertical
the vector is defined to be vertical
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.