SimBcPlotContoursBuilderPlotType Enumeration

NXOpen.CAE.SimBcPlotContoursBuilder.PlotType is an alias for NXOpen.CAE.SimBcPlotContoursBuilderPlotType

class NXOpen.CAE.SimBcPlotContoursBuilderPlotType

Bases: object

Plot types

Enum Members

Enum Member Enum Member Description
Static
Static plot
Animation
Animation
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.