LaminateImportedLayupBuilderApiTypeEnum Enumeration

NXOpen.CAE.LaminateImportedLayupBuilder.ApiTypeEnum is an alias for NXOpen.CAE.LaminateImportedLayupBuilderApiTypeEnum

class NXOpen.CAE.LaminateImportedLayupBuilderApiTypeEnum

Bases: object

Type of external API supported.

Only FiberSim API for now.

Enum Members

Enum Member Enum Member Description
FiberSim
FiberSIM layup XML file.
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.