LaminateGraphicalReportBuilderPlyExportOptionType Enumeration

NXOpen.CAE.LaminateGraphicalReportBuilder.PlyExportOptionType is an alias for NXOpen.CAE.LaminateGraphicalReportBuilderPlyExportOptionType

class NXOpen.CAE.LaminateGraphicalReportBuilderPlyExportOptionType

Bases: object

Ply export options.

With or without ply ids.

Enum Members

Enum Member Enum Member Description
GlobalPlyId
Export the ply global ids to the bun file
Layer
Export plies as layers
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.