ResultMeasureModelSubsetFE Class¶
-
class
NXOpen.CAE.
ResultMeasureModelSubsetFE
¶ Bases:
NXOpen.CAE.ResultMeasureModelSubset
Represents a FE-based subset of the model upon which to calculate results
To obtain an instance of this class use
NXOpen.CAE.ResultMeasureCollection()
.New in version NX8.5.0.
Methods¶
Method | Description |
---|---|
Dispose | Frees the object from memory. |
SetElements | Set the finite elements |
SetNodes | Set the nodes |
Method Detail¶
Dispose¶
-
ResultMeasureModelSubsetFE.
Dispose
¶ Frees the object from memory.
After this method is called, it is illegal to use the object. In .NET, this method is automatically called when the object is deleted by the garbage collector.
Signature
Dispose()
New in version NX8.5.0.
License requirements: None.
SetElements¶
-
ResultMeasureModelSubsetFE.
SetElements
¶ Set the finite elements
Signature
SetElements(elements)
Parameters: elements (list of NXOpen.CAE.FEElement
) –New in version NX8.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
SetNodes¶
-
ResultMeasureModelSubsetFE.
SetNodes
¶ Set the nodes
Signature
SetNodes(elements)
Parameters: elements (list of NXOpen.CAE.FENode
) –New in version NX8.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)