DurabilityEventFatigueSettingsBuilder Class¶
-
class
NXOpen.CAE.
DurabilityEventFatigueSettingsBuilder
¶ Bases:
NXOpen.Builder
Represents a builder class for the event fatigue settings.
The fatigue settings help the user control the fatigue/durability parameters in the event. To create a new instance of this class, use
NXOpen.CAE.DurabilityFatigueCollection.CreateEventfatiguesettingsBuilder()
New in version NX7.5.0.
Properties¶
Property | Description |
---|---|
BwiWeldClass | Returns or sets the bwi weld class. |
CyclesToFailure | Returns or sets the cycles to failure. |
CyclicStressStrainModel | Returns or sets the cyclic stress strain model. |
EquivalentStressMethod | Returns or sets the equivalent stress method. |
EventDamage | Returns or sets the event damage. |
EventDamageDirection | Returns or sets the event damage direction. |
EventLife | Returns or sets the event life. |
FailureIndex | Returns or sets the failure index. |
FatigueLifeCriterion | Returns or sets the fatigue life criterion. |
FatigueSafetyFactorKeyin | Returns or sets the fatigue safety factor keyin. |
FatigueSafetyFactorMethod | Returns or sets the fatigue safety factor method. |
FatigueSafetyFactorOutput | Returns or sets the fatigue safety factor output. |
FatigueSafetyFactorToggle | Returns or sets the fatigue safety factor toggle. |
FreeFaceIndicator | Returns or sets the free face indicator. |
IncludeMeanStressEffects | Returns or sets the include mean stress effects. |
LoadProportionality | Returns or sets the load proportionality. |
MaximumAlternatingStress | Returns or sets the maximum alternating stress. |
MaximumAlternatingStressKeyin | Returns the maximum alternating stress keyin. |
Name | Returns or sets the name. |
NotchFactor | Returns or sets the notch factor. |
NumberOfElementsInHysterisisLoop | Returns or sets the number of elements in hysterisis loop. |
NumberOfOccurrences | Returns or sets the number of occurrences. |
NumberOfStandardDeviations | Returns or sets the number of standard deviations. |
OrthotropicFatigueCriterion | Returns or sets the orthotropic fatigue criterion. |
OrthotropicMeanStress | Returns or sets the orthotropic mean stress. |
PerformOrthotropicAnalysis | Returns or sets the perform orthropic analysis. |
PlateThicknessExponent | Returns or sets the plate thickness exponent. |
PlateThicknessRatio | Returns or sets the plate thickness ratio. |
PrincipalAxisStability | Returns or sets the principal axis stability. |
ProbabilityOfFailure | Returns or sets the probability of failure. |
ProbabilityOption | Returns or sets the probability distribution. |
Tag | Returns the Tag for this object. |
TwiHighCycleCutoff | Returns or sets the twi high cycle cutoff. |
TwiHighCycleSlopeChange | Returns or sets the twi high cycle slope change. |
TwiLowCycleStressCutoff | Returns or sets the twi low cycle stress cutoff. |
TwiLowCycleStressExtension | Returns or sets the twi low cycle stress extension. |
UseNotchFactor | Returns or sets the use notch factor. |
UsePlateThicknessCorrection | Returns or sets the plate thickness correction usage. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
Property Detail¶
BwiWeldClass¶
-
DurabilityEventFatigueSettingsBuilder.
BwiWeldClass
¶ Returns or sets the bwi weld class.
-------------------------------------
Getter Method
Signature
BwiWeldClass()
Returns: Return type: NXOpen.CAE.DurabilityEventFatigueSettingsBuilderBwiWeldClassEnum
New in version NX7.5.2.
License requirements: None.
-------------------------------------
Setter Method
Signature
BwiWeldClass(bwiWeldClass)
Parameters: bwiWeldClass ( NXOpen.CAE.DurabilityEventFatigueSettingsBuilderBwiWeldClassEnum
) –New in version NX7.5.2.
License requirements: nx_adv_durability (“NX Advanced Durability”)
CyclesToFailure¶
-
DurabilityEventFatigueSettingsBuilder.
CyclesToFailure
¶ Returns or sets the cycles to failure.
-------------------------------------
Getter Method
Signature
CyclesToFailure()
Returns: Return type: float New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CyclesToFailure(cyclesToFailure)
Parameters: cyclesToFailure (float) – New in version NX7.5.0.
License requirements: nx_adv_durability (“NX Advanced Durability”)
CyclicStressStrainModel¶
-
DurabilityEventFatigueSettingsBuilder.
CyclicStressStrainModel
¶ Returns or sets the cyclic stress strain model.
-------------------------------------
Getter Method
Signature
CyclicStressStrainModel()
Returns: Return type: NXOpen.CAE.DurabilityEventFatigueSettingsBuilderCyclicStressStrainModelEnum
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CyclicStressStrainModel(cyclicStressStrainModel)
Parameters: cyclicStressStrainModel ( NXOpen.CAE.DurabilityEventFatigueSettingsBuilderCyclicStressStrainModelEnum
) –New in version NX7.5.0.
License requirements: nx_adv_durability (“NX Advanced Durability”)
EquivalentStressMethod¶
-
DurabilityEventFatigueSettingsBuilder.
EquivalentStressMethod
¶ Returns or sets the equivalent stress method.
-------------------------------------
Getter Method
Signature
EquivalentStressMethod()
Returns: Return type: NXOpen.CAE.DurabilityEventFatigueSettingsBuilderEquivalentStressMethodEnum
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
EquivalentStressMethod(equivalentStressMethod)
Parameters: equivalentStressMethod ( NXOpen.CAE.DurabilityEventFatigueSettingsBuilderEquivalentStressMethodEnum
) –New in version NX7.5.0.
License requirements: nx_adv_durability (“NX Advanced Durability”)
EventDamage¶
-
DurabilityEventFatigueSettingsBuilder.
EventDamage
¶ Returns or sets the event damage.
-------------------------------------
Getter Method
Signature
EventDamage()
Returns: Return type: bool New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
EventDamage(eventDamage)
Parameters: eventDamage (bool) – New in version NX7.5.0.
License requirements: nx_adv_durability (“NX Advanced Durability”)
EventDamageDirection¶
-
DurabilityEventFatigueSettingsBuilder.
EventDamageDirection
¶ Returns or sets the event damage direction.
-------------------------------------
Getter Method
Signature
EventDamageDirection()
Returns: Return type: bool New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
EventDamageDirection(eventDamageDirection)
Parameters: eventDamageDirection (bool) – New in version NX9.0.0.
License requirements: nx_adv_durability (“NX Advanced Durability”)
EventLife¶
-
DurabilityEventFatigueSettingsBuilder.
EventLife
¶ Returns or sets the event life.
-------------------------------------
Getter Method
Signature
EventLife()
Returns: Return type: bool New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
EventLife(eventLife)
Parameters: eventLife (bool) – New in version NX7.5.0.
License requirements: nx_adv_durability (“NX Advanced Durability”)
FailureIndex¶
-
DurabilityEventFatigueSettingsBuilder.
FailureIndex
¶ Returns or sets the failure index.
-------------------------------------
Getter Method
Signature
FailureIndex()
Returns: Return type: bool New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
FailureIndex(failureIndex)
Parameters: failureIndex (bool) – New in version NX7.5.0.
License requirements: nx_adv_durability (“NX Advanced Durability”)
FatigueLifeCriterion¶
-
DurabilityEventFatigueSettingsBuilder.
FatigueLifeCriterion
¶ Returns or sets the fatigue life criterion.
-------------------------------------
Getter Method
Signature
FatigueLifeCriterion()
Returns: Return type: NXOpen.CAE.DurabilityEventFatigueSettingsBuilderFatigueLifeCriterionEnum
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
FatigueLifeCriterion(fatigueLifeCriterion)
Parameters: fatigueLifeCriterion ( NXOpen.CAE.DurabilityEventFatigueSettingsBuilderFatigueLifeCriterionEnum
) –New in version NX7.5.0.
License requirements: nx_adv_durability (“NX Advanced Durability”)
FatigueSafetyFactorKeyin¶
-
DurabilityEventFatigueSettingsBuilder.
FatigueSafetyFactorKeyin
¶ Returns or sets the fatigue safety factor keyin.
-------------------------------------
Getter Method
Signature
FatigueSafetyFactorKeyin()
Returns: Return type: float New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
FatigueSafetyFactorKeyin(fatigueSafetyFactorKeyin)
Parameters: fatigueSafetyFactorKeyin (float) – New in version NX7.5.0.
License requirements: nx_adv_durability (“NX Advanced Durability”)
FatigueSafetyFactorMethod¶
-
DurabilityEventFatigueSettingsBuilder.
FatigueSafetyFactorMethod
¶ Returns or sets the fatigue safety factor method.
-------------------------------------
Getter Method
Signature
FatigueSafetyFactorMethod()
Returns: Return type: NXOpen.CAE.DurabilityEventFatigueSettingsBuilderFatigueSafetyFactorMethodEnum
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
FatigueSafetyFactorMethod(fatigueSafetyFactorMethod)
Parameters: fatigueSafetyFactorMethod ( NXOpen.CAE.DurabilityEventFatigueSettingsBuilderFatigueSafetyFactorMethodEnum
) –New in version NX7.5.0.
License requirements: nx_adv_durability (“NX Advanced Durability”)
FatigueSafetyFactorOutput¶
-
DurabilityEventFatigueSettingsBuilder.
FatigueSafetyFactorOutput
¶ Returns or sets the fatigue safety factor output.
-------------------------------------
Getter Method
Signature
FatigueSafetyFactorOutput()
Returns: Return type: NXOpen.CAE.DurabilityEventFatigueSettingsBuilderFatigueSafetyFactorOutputEnum
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
FatigueSafetyFactorOutput(fatigueSafetyFactorOutput)
Parameters: fatigueSafetyFactorOutput ( NXOpen.CAE.DurabilityEventFatigueSettingsBuilderFatigueSafetyFactorOutputEnum
) –New in version NX7.5.0.
License requirements: nx_adv_durability (“NX Advanced Durability”)
FatigueSafetyFactorToggle¶
-
DurabilityEventFatigueSettingsBuilder.
FatigueSafetyFactorToggle
¶ Returns or sets the fatigue safety factor toggle.
-------------------------------------
Getter Method
Signature
FatigueSafetyFactorToggle()
Returns: Return type: bool New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
FatigueSafetyFactorToggle(fatigueSafetyFactorToggle)
Parameters: fatigueSafetyFactorToggle (bool) – New in version NX7.5.0.
License requirements: nx_adv_durability (“NX Advanced Durability”)
FreeFaceIndicator¶
-
DurabilityEventFatigueSettingsBuilder.
FreeFaceIndicator
¶ Returns or sets the free face indicator.
-------------------------------------
Getter Method
Signature
FreeFaceIndicator()
Returns: Return type: bool New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
FreeFaceIndicator(freeFaceIndicator)
Parameters: freeFaceIndicator (bool) – New in version NX9.0.0.
License requirements: nx_adv_durability (“NX Advanced Durability”)
IncludeMeanStressEffects¶
-
DurabilityEventFatigueSettingsBuilder.
IncludeMeanStressEffects
¶ Returns or sets the include mean stress effects.
-------------------------------------
Getter Method
Signature
IncludeMeanStressEffects()
Returns: Return type: bool New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
IncludeMeanStressEffects(includeMeanStressEffects)
Parameters: includeMeanStressEffects (bool) – New in version NX7.5.0.
License requirements: nx_adv_durability (“NX Advanced Durability”)
LoadProportionality¶
-
DurabilityEventFatigueSettingsBuilder.
LoadProportionality
¶ Returns or sets the load proportionality.
-------------------------------------
Getter Method
Signature
LoadProportionality()
Returns: Return type: bool New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
LoadProportionality(loadProportionality)
Parameters: loadProportionality (bool) – New in version NX9.0.0.
License requirements: nx_adv_durability (“NX Advanced Durability”)
MaximumAlternatingStress¶
-
DurabilityEventFatigueSettingsBuilder.
MaximumAlternatingStress
¶ Returns or sets the maximum alternating stress.
-------------------------------------
Getter Method
Signature
MaximumAlternatingStress()
Returns: Return type: NXOpen.CAE.DurabilityEventFatigueSettingsBuilderMaximumAlternatingStressEnum
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
MaximumAlternatingStress(maximumAlternatingStress)
Parameters: maximumAlternatingStress ( NXOpen.CAE.DurabilityEventFatigueSettingsBuilderMaximumAlternatingStressEnum
) –New in version NX7.5.0.
License requirements: nx_adv_durability (“NX Advanced Durability”)
MaximumAlternatingStressKeyin¶
-
DurabilityEventFatigueSettingsBuilder.
MaximumAlternatingStressKeyin
¶ Returns the maximum alternating stress keyin.
-------------------------------------
Getter Method
Signature
MaximumAlternatingStressKeyin()
Returns: Return type: NXOpen.Expression
New in version NX7.5.0.
License requirements: None.
Name¶
-
DurabilityEventFatigueSettingsBuilder.
Name
¶ Returns or sets the name.
-------------------------------------
Getter Method
Signature
Name()
Returns: Return type: str New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Name(title)
Parameters: title (str) – New in version NX8.5.0.
License requirements: nx_adv_durability (“NX Advanced Durability”)
NotchFactor¶
-
DurabilityEventFatigueSettingsBuilder.
NotchFactor
¶ Returns or sets the notch factor.
-------------------------------------
Getter Method
Signature
NotchFactor()
Returns: Return type: float New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
NotchFactor(notchFactor)
Parameters: notchFactor (float) – New in version NX7.5.0.
License requirements: nx_adv_durability (“NX Advanced Durability”)
NumberOfElementsInHysterisisLoop¶
-
DurabilityEventFatigueSettingsBuilder.
NumberOfElementsInHysterisisLoop
¶ Returns or sets the number of elements in hysterisis loop.
-------------------------------------
Getter Method
Signature
NumberOfElementsInHysterisisLoop()
Returns: Return type: int New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
NumberOfElementsInHysterisisLoop(numberOfElementsInHysterisisLoop)
Parameters: numberOfElementsInHysterisisLoop (int) – New in version NX7.5.0.
License requirements: nx_adv_durability (“NX Advanced Durability”)
NumberOfOccurrences¶
-
DurabilityEventFatigueSettingsBuilder.
NumberOfOccurrences
¶ Returns or sets the number of occurrences.
-------------------------------------
Getter Method
Signature
NumberOfOccurrences()
Returns: Return type: int New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
NumberOfOccurrences(numberOfOccurrences)
Parameters: numberOfOccurrences (int) – New in version NX7.5.0.
License requirements: nx_adv_durability (“NX Advanced Durability”)
NumberOfStandardDeviations¶
-
DurabilityEventFatigueSettingsBuilder.
NumberOfStandardDeviations
¶ Returns or sets the number of standard deviations.
-------------------------------------
Getter Method
Signature
NumberOfStandardDeviations()
Returns: Return type: float New in version NX7.5.2.
License requirements: None.
-------------------------------------
Setter Method
Signature
NumberOfStandardDeviations(numberOfStandardDeviations)
Parameters: numberOfStandardDeviations (float) – New in version NX7.5.2.
License requirements: nx_adv_durability (“NX Advanced Durability”)
OrthotropicFatigueCriterion¶
-
DurabilityEventFatigueSettingsBuilder.
OrthotropicFatigueCriterion
¶ Returns or sets the orthotropic fatigue criterion.
-------------------------------------
Getter Method
Signature
OrthotropicFatigueCriterion()
Returns: Return type: NXOpen.CAE.DurabilityEventFatigueSettingsBuilderOrthotropicFatigueCriterionEnum
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
OrthotropicFatigueCriterion(orthotropicFatigueCriterion)
Parameters: orthotropicFatigueCriterion ( NXOpen.CAE.DurabilityEventFatigueSettingsBuilderOrthotropicFatigueCriterionEnum
) –New in version NX9.0.0.
License requirements: nx_adv_durability (“NX Advanced Durability”)
OrthotropicMeanStress¶
-
DurabilityEventFatigueSettingsBuilder.
OrthotropicMeanStress
¶ Returns or sets the orthotropic mean stress.
-------------------------------------
Getter Method
Signature
OrthotropicMeanStress()
Returns: Return type: NXOpen.CAE.DurabilityEventFatigueSettingsBuilderOrthotropicMeanStressEnum
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
OrthotropicMeanStress(orthotropicMeanStress)
Parameters: orthotropicMeanStress ( NXOpen.CAE.DurabilityEventFatigueSettingsBuilderOrthotropicMeanStressEnum
) –New in version NX9.0.0.
License requirements: nx_adv_durability (“NX Advanced Durability”)
PerformOrthotropicAnalysis¶
-
DurabilityEventFatigueSettingsBuilder.
PerformOrthotropicAnalysis
¶ Returns or sets the perform orthropic analysis.
-------------------------------------
Getter Method
Signature
PerformOrthotropicAnalysis()
Returns: Return type: bool New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PerformOrthotropicAnalysis(performOrthotropicAnalysis)
Parameters: performOrthotropicAnalysis (bool) – New in version NX9.0.0.
License requirements: nx_adv_durability (“NX Advanced Durability”)
PlateThicknessExponent¶
-
DurabilityEventFatigueSettingsBuilder.
PlateThicknessExponent
¶ Returns or sets the plate thickness exponent.
-------------------------------------
Getter Method
Signature
PlateThicknessExponent()
Returns: Return type: float New in version NX7.5.2.
License requirements: None.
-------------------------------------
Setter Method
Signature
PlateThicknessExponent(plateThicknessExponent)
Parameters: plateThicknessExponent (float) – New in version NX7.5.2.
License requirements: nx_adv_durability (“NX Advanced Durability”)
PlateThicknessRatio¶
-
DurabilityEventFatigueSettingsBuilder.
PlateThicknessRatio
¶ Returns or sets the plate thickness ratio.
-------------------------------------
Getter Method
Signature
PlateThicknessRatio()
Returns: Return type: float New in version NX7.5.2.
License requirements: None.
-------------------------------------
Setter Method
Signature
PlateThicknessRatio(plateThicknessRatio)
Parameters: plateThicknessRatio (float) – New in version NX7.5.2.
License requirements: nx_adv_durability (“NX Advanced Durability”)
PrincipalAxisStability¶
-
DurabilityEventFatigueSettingsBuilder.
PrincipalAxisStability
¶ Returns or sets the principal axis stability.
-------------------------------------
Getter Method
Signature
PrincipalAxisStability()
Returns: Return type: bool New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PrincipalAxisStability(principalAxisStability)
Parameters: principalAxisStability (bool) – New in version NX9.0.0.
License requirements: nx_adv_durability (“NX Advanced Durability”)
ProbabilityOfFailure¶
-
DurabilityEventFatigueSettingsBuilder.
ProbabilityOfFailure
¶ Returns or sets the probability of failure.
-------------------------------------
Getter Method
Signature
ProbabilityOfFailure()
Returns: Return type: float New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ProbabilityOfFailure(probabilityOfFailure)
Parameters: probabilityOfFailure (float) – New in version NX8.0.0.
License requirements: nx_adv_durability (“NX Advanced Durability”)
ProbabilityOption¶
-
DurabilityEventFatigueSettingsBuilder.
ProbabilityOption
¶ Returns or sets the probability distribution.
-------------------------------------
Getter Method
Signature
ProbabilityOption()
Returns: Return type: NXOpen.CAE.DurabilityEventFatigueSettingsBuilderProbabilityOptionEnum
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ProbabilityOption(probabilityOption)
Parameters: probabilityOption ( NXOpen.CAE.DurabilityEventFatigueSettingsBuilderProbabilityOptionEnum
) –New in version NX8.0.0.
License requirements: nx_adv_durability (“NX Advanced Durability”)
TwiHighCycleCutoff¶
-
DurabilityEventFatigueSettingsBuilder.
TwiHighCycleCutoff
¶ Returns or sets the twi high cycle cutoff.
-------------------------------------
Getter Method
Signature
TwiHighCycleCutoff()
Returns: Return type: float New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
TwiHighCycleCutoff(twiHighCycleCutoff)
Parameters: twiHighCycleCutoff (float) – New in version NX8.0.0.
License requirements: nx_adv_durability (“NX Advanced Durability”)
TwiHighCycleSlopeChange¶
-
DurabilityEventFatigueSettingsBuilder.
TwiHighCycleSlopeChange
¶ Returns or sets the twi high cycle slope change.
-------------------------------------
Getter Method
Signature
TwiHighCycleSlopeChange()
Returns: Return type: float New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
TwiHighCycleSlopeChange(twiHighCycleSlopeChange)
Parameters: twiHighCycleSlopeChange (float) – New in version NX8.0.0.
License requirements: nx_adv_durability (“NX Advanced Durability”)
TwiLowCycleStressCutoff¶
-
DurabilityEventFatigueSettingsBuilder.
TwiLowCycleStressCutoff
¶ Returns or sets the twi low cycle stress cutoff.
-------------------------------------
Getter Method
Signature
TwiLowCycleStressCutoff()
Returns: Return type: float New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
TwiLowCycleStressCutoff(twiLowCycleStressCutoff)
Parameters: twiLowCycleStressCutoff (float) – New in version NX8.0.0.
License requirements: nx_adv_durability (“NX Advanced Durability”)
TwiLowCycleStressExtension¶
-
DurabilityEventFatigueSettingsBuilder.
TwiLowCycleStressExtension
¶ Returns or sets the twi low cycle stress extension.
-------------------------------------
Getter Method
Signature
TwiLowCycleStressExtension()
Returns: Return type: float New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
TwiLowCycleStressExtension(twiLowCycleStressExtension)
Parameters: twiLowCycleStressExtension (float) – New in version NX8.0.0.
License requirements: nx_adv_durability (“NX Advanced Durability”)
UseNotchFactor¶
-
DurabilityEventFatigueSettingsBuilder.
UseNotchFactor
¶ Returns or sets the use notch factor.
-------------------------------------
Getter Method
Signature
UseNotchFactor()
Returns: Return type: bool New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
UseNotchFactor(useNotchFactor)
Parameters: useNotchFactor (bool) – New in version NX7.5.0.
License requirements: nx_adv_durability (“NX Advanced Durability”)
UsePlateThicknessCorrection¶
-
DurabilityEventFatigueSettingsBuilder.
UsePlateThicknessCorrection
¶ Returns or sets the plate thickness correction usage.
-------------------------------------
Getter Method
Signature
UsePlateThicknessCorrection()
Returns: Return type: bool New in version NX7.5.2.
License requirements: None.
-------------------------------------
Setter Method
Signature
UsePlateThicknessCorrection(usePlateThicknessCorrection)
Parameters: usePlateThicknessCorrection (bool) – New in version NX7.5.2.
License requirements: nx_adv_durability (“NX Advanced Durability”)
Method Detail¶
Validate¶
-
DurabilityEventFatigueSettingsBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.