DurabilityEventFatigueSettingsBuilderMaximumAlternatingStressEnum Enumeration

NXOpen.CAE.DurabilityEventFatigueSettingsBuilder.MaximumAlternatingStressEnum is an alias for NXOpen.CAE.DurabilityEventFatigueSettingsBuilderMaximumAlternatingStressEnum

class NXOpen.CAE.DurabilityEventFatigueSettingsBuilderMaximumAlternatingStressEnum

Bases: object

the Maximum Alternating Stress Enum.

Enum Members

Enum Member Enum Member Description
Calculate
Calculate
Keyin
Keyin
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.