DurabilityEventFatigueSettingsBuilderFatigueLifeCriterionEnum Enumeration

NXOpen.CAE.DurabilityEventFatigueSettingsBuilder.FatigueLifeCriterionEnum is an alias for NXOpen.CAE.DurabilityEventFatigueSettingsBuilderFatigueLifeCriterionEnum

class NXOpen.CAE.DurabilityEventFatigueSettingsBuilderFatigueLifeCriterionEnum

Bases: object

the fatigue life criterion enum.

Enum Members

Enum Member Enum Member Description
SmithWatsonTopper
SWT
StrainLifeMaximumPrincipal
Maximum Principal
StrainLifeMaximumShear
Maximum Shear
StressLife
Stress Life
Bwi
BWI
Twi
TWI
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.