DurabilityEventFatigueSettingsBuilderBwiWeldClassEnum Enumeration

NXOpen.CAE.DurabilityEventFatigueSettingsBuilder.BwiWeldClassEnum is an alias for NXOpen.CAE.DurabilityEventFatigueSettingsBuilderBwiWeldClassEnum

class NXOpen.CAE.DurabilityEventFatigueSettingsBuilderBwiWeldClassEnum

Bases: object

the BWi Weld Class Enum.

Enum Members

Enum Member Enum Member Description
B
B
C
C
D
D
E
E
F
F
F2
F2
G
G
W
W
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.