CorrelFineTuneAlignmentBuilder Class¶
-
class
NXOpen.CAE.
CorrelFineTuneAlignmentBuilder
¶ Bases:
NXOpen.CAE.CorrelBaseBuilder
This builder is used to nudge the alignment by a fine adjustment
To create a new instance of this class, use
NXOpen.CAE.CorrelManager.CreateCorrelFineTuneAlignmentBuilder()
New in version NX9.0.0.
Properties¶
Property | Description |
---|---|
AngleEnum | Returns or sets the angle vector enumeration |
AngularExp | Returns the angular expression |
DistanceEnum | Returns or sets the distance vector enumeration |
DistanceExp | Returns the distance expression |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
MoveButton | The move button to nudge alignment by the defined distance along the selected distance vector |
RotateButton | The rotate button to nudge alignment by the defined angle via the selected angle vector |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
CorrelFineTuneAlignmentBuilderAngleVector Enumeration | the angle vector enumeration for the alignment nudge |
CorrelFineTuneAlignmentBuilderDistanceVector Enumeration | the distance vector enumeration for the alignment nudge |
Property Detail¶
AngleEnum¶
-
CorrelFineTuneAlignmentBuilder.
AngleEnum
¶ Returns or sets the angle vector enumeration
-------------------------------------
Getter Method
Signature
AngleEnum()
Returns: Return type: NXOpen.CAE.CorrelFineTuneAlignmentBuilderAngleVector
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AngleEnum(angleEnum)
Parameters: angleEnum ( NXOpen.CAE.CorrelFineTuneAlignmentBuilderAngleVector
) –New in version NX9.0.0.
License requirements: nx_correl_base (“FE Correlation”)
AngularExp¶
-
CorrelFineTuneAlignmentBuilder.
AngularExp
¶ Returns the angular expression
-------------------------------------
Getter Method
Signature
AngularExp()
Returns: Return type: NXOpen.Expression
New in version NX9.0.0.
License requirements: None.
DistanceEnum¶
-
CorrelFineTuneAlignmentBuilder.
DistanceEnum
¶ Returns or sets the distance vector enumeration
-------------------------------------
Getter Method
Signature
DistanceEnum()
Returns: Return type: NXOpen.CAE.CorrelFineTuneAlignmentBuilderDistanceVector
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DistanceEnum(distanceEnum)
Parameters: distanceEnum ( NXOpen.CAE.CorrelFineTuneAlignmentBuilderDistanceVector
) –New in version NX9.0.0.
License requirements: nx_correl_base (“FE Correlation”)
DistanceExp¶
-
CorrelFineTuneAlignmentBuilder.
DistanceExp
¶ Returns the distance expression
-------------------------------------
Getter Method
Signature
DistanceExp()
Returns: Return type: NXOpen.Expression
New in version NX9.0.0.
License requirements: None.
Method Detail¶
MoveButton¶
-
CorrelFineTuneAlignmentBuilder.
MoveButton
¶ The move button to nudge alignment by the defined distance along the selected distance vector
Signature
MoveButton()
New in version NX9.0.0.
License requirements: nx_correl_base (“FE Correlation”)
RotateButton¶
-
CorrelFineTuneAlignmentBuilder.
RotateButton
¶ The rotate button to nudge alignment by the defined angle via the selected angle vector
Signature
RotateButton()
New in version NX9.0.0.
License requirements: nx_correl_base (“FE Correlation”)
Validate¶
-
CorrelFineTuneAlignmentBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.