AfuMathOperationOverall Enumeration

NXOpen.CAE.AfuMathOperation.Overall is an alias for NXOpen.CAE.AfuMathOperationOverall

class NXOpen.CAE.AfuMathOperationOverall

Bases: object

Defines the type of Overall Math Operations

Enum Members

Enum Member Enum Member Description
MinimumValue
Gets minimum values of AFU records
MaximumValue
Gets maximum values of AFU records
MinimumMagnitude
Gets minimum magnitude values of AFU records
MaximumMagnitude
Gets maximum magnitude values of AFU records
MeanMagnitude
Gets mean magnitude values of AFU records
SumMagnitude
Gets sum magnitude values of AFU records
SumComplex
Gets complex sum values of AFU records
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.