BeamSectionDirectionOption Enumeration

NXOpen.CAE.BeamSection.DirectionOption is an alias for NXOpen.CAE.BeamSectionDirectionOption

class NXOpen.CAE.BeamSectionDirectionOption

Bases: object

Represents the direction

Enum Members

Enum Member Enum Member Description
Horizontal
Indicates the horizontal direction of beam section
Vertical
Indicates the vertical direction of beam section
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.