Iteration Class¶
-
class
NXOpen.CAE.
Iteration
¶ Bases:
NXOpen.CAE.BaseIteration
Represents iteration present in a
NXOpen.CAE.Loadcase
.Iterations can not be created externally as these cases comes from the result file
An instance of this class can not be obtained
New in version NX7.5.0.
Properties¶
Property | Description |
---|---|
Label | Returns the identifier of the iteration that comes from a result file |
Name | Returns the name of the iteration |
Tag | Returns the Tag for this object. |
Type | Returns the type of the iteration |
Unit | Returns the units for the iteration value |
Value | Returns the iteration value |
ValueType | Returns the iteration value type |
Methods¶
Method | Description |
---|---|
Find | Returns a NXOpen.CAE.BaseResultType @return |
GetResultTypes | Returns the result types present in this iteration @return |
GetSubIterations | Returns the sub iterations present in this iteration @return |
Property Detail¶
Label¶
-
Iteration.
Label
¶ Returns the identifier of the iteration that comes from a result file
-------------------------------------
Getter Method
Signature
Label()
Returns: Return type: int New in version NX7.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)