Loadcase Class¶
-
class
NXOpen.CAE.
Loadcase
¶ Bases:
NXOpen.CAE.BaseLoadcase
Represents loadcases present in a
NXOpen.CAE.Result
.Loadcases can not be created externally as these cases comes from the result file
An instance of this class can not be obtained
New in version NX7.5.0.
Properties¶
Property | Description |
---|---|
Label | Returns the identifier of the loadcase that comes from a result file |
Name | Returns the NX assigned name of the loadcase |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Find | Returns a NXOpen.CAE.BaseIteration @return |
GetIterations | Get iteration present in this loadcase @return |
Property Detail¶
Label¶
-
Loadcase.
Label
¶ Returns the identifier of the loadcase that comes from a result file
-------------------------------------
Getter Method
Signature
Label()
Returns: Return type: int New in version NX7.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)