LaminatePlyCollection Class¶
-
class
NXOpen.CAE.
LaminatePlyCollection
¶ Bases:
object
Represents a list of plies, which have a material, a thickness, an orientation, and a color
. To obtain an instance of this class, refer to
NXOpen.CAE.LaminatePlyGroup
New in version NX5.0.0.
Methods¶
Method | Description |
---|---|
DeletePly | Deletes an existing NXOpen.CAE.LaminatePly |
FindObject | Finds the NXOpen.CAE.LaminatePly with the given identifier as recorded in a journal. |
GetPly | Retrieve the ply at specified index @return |
InsertCohesiveLayer | Inserts a new cohesive layer in the group @return Layer created |
InsertPly | Inserts a new single NXOpen.CAE.LaminatePly @return Ply created |
Method Detail¶
DeletePly¶
-
LaminatePlyCollection.
DeletePly
¶ Deletes an existing
NXOpen.CAE.LaminatePly
Signature
DeletePly(index)
Parameters: index (int) – Index in group of ply to delete New in version NX5.0.0.
License requirements: nx_lam_composites (“Laminate Composites”)
FindObject¶
-
LaminatePlyCollection.
FindObject
¶ Finds the
NXOpen.CAE.LaminatePly
with the given identifier as recorded in a journal.An exception will be thrown if no object can be found with the given journal identifier.
Signature
FindObject(journalIdentifier)
Parameters: journalIdentifier (str) – Identifier to be found Returns: ply found Return type: NXOpen.CAE.LaminatePly
New in version NX7.5.0.
License requirements: nx_lam_composites (“Laminate Composites”)
GetPly¶
-
LaminatePlyCollection.
GetPly
¶ Retrieve the ply at specified index
Signature
GetPly(plyIndex)
Parameters: plyIndex (int) – ply number of interest Returns: Return type: NXOpen.CAE.LaminatePly
New in version NX5.0.0.
License requirements: nx_lam_composites (“Laminate Composites”)
InsertCohesiveLayer¶
-
LaminatePlyCollection.
InsertCohesiveLayer
¶ Inserts a new cohesive layer in the group
Signature
InsertCohesiveLayer(insertionIndex, orientation, color)
Parameters: - insertionIndex (int) – Index where layer is inserted
- orientation (float) – Orientation of the layer
- color (int) – Layer color
Returns: Layer created
Return type: New in version NX10.0.0.
License requirements: nx_lam_composites (“Laminate Composites”)
InsertPly¶
-
LaminatePlyCollection.
InsertPly
¶ Inserts a new single
NXOpen.CAE.LaminatePly
Signature
InsertPly(insertionIndex, thickness, orientation, color)
Parameters: - insertionIndex (int) – Index where ply is inserted
- thickness (float) – Thickness of the ply
- orientation (float) – Orientation of the ply
- color (int) – Ply color
Returns: Ply created
Return type: New in version NX5.0.0.
License requirements: nx_lam_composites (“Laminate Composites”)