LaminateElementFilterBuilder Class

class NXOpen.CAE.LaminateElementFilterBuilder

Bases: NXOpen.Builder

Represents a NXOpen.CAE.LaminateGraphicalReport builder

There is no kf creator.

New in version NX8.0.0.

Properties

Property Description
SelectAllElements Returns or sets the select all elements option
SelectElements Returns the selected elements
Tag Returns the Tag for this object.

Methods

Method Description
Commit Commits any edits that have been applied to the builder.
Destroy Deletes the builder, and cleans up any objects created by the builder.
GetCommittedObjects For builders that create more than one object, this method returns the objects that are created by commit.
GetObject Returns the object currently being edited by this builder.
ShowResults Updates the model to reflect the result of an edit to the model for all builders that support showing results.
Validate Validate whether the inputs to the component are sufficient for commit to be called.

Property Detail

SelectAllElements

LaminateElementFilterBuilder.SelectAllElements

Returns or sets the select all elements option

-------------------------------------

Getter Method

Signature SelectAllElements()

Returns:
Return type:bool

New in version NX8.0.0.

License requirements: nx_lam_composites (“Laminate Composites”)

-------------------------------------

Setter Method

Signature SelectAllElements(selectAllElements)

Parameters:selectAllElements (bool) –

New in version NX8.0.0.

License requirements: nx_lam_composites (“Laminate Composites”)

SelectElements

LaminateElementFilterBuilder.SelectElements

Returns the selected elements

-------------------------------------

Getter Method

Signature SelectElements()

Returns:
Return type:NXOpen.CAE.SelectElementsBuilder

New in version NX8.0.0.

License requirements: nx_lam_composites (“Laminate Composites”)

Method Detail

Validate

LaminateElementFilterBuilder.Validate

Validate whether the inputs to the component are sufficient for commit to be called.

If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.

Signature Validate()

Returns:Was self validation successful
Return type:bool

New in version NX3.0.1.

License requirements: None.