PreTestExciterConfigCollection Class¶
-
class
NXOpen.CAE.
PreTestExciterConfigCollection
¶ Bases:
object
Represents a collection of exciter selection configuration
To obtain an instance of this class, refer to
NXOpen.CAE.PreTestExciterSelectionControl
New in version NX8.0.0.
Properties¶
Property | Description |
---|---|
ActiveExciterConfig | Returns or sets the pre-test active exciter configuration |
Methods¶
Method | Description |
---|---|
CloneExciterConfig | Clone a pre-test exciter configuration @return Cloned Pre-Test exciter configuration |
FindObject | Finds a exciter selection configuration with specified name @return exciter selection configuration found |
RemoveExciterConfig | Removes and deletes a exciter selection configuration |
Property Detail¶
ActiveExciterConfig¶
-
PreTestExciterConfigCollection.
ActiveExciterConfig
¶ Returns or sets the pre-test active exciter configuration
-------------------------------------
Getter Method
Signature
ActiveExciterConfig()
Returns: Return type: int New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ActiveExciterConfig(activeConfig)
Parameters: activeConfig (int) – New in version NX8.0.0.
License requirements: nx_correl_base (“FE Correlation”)
Method Detail¶
CloneExciterConfig¶
-
PreTestExciterConfigCollection.
CloneExciterConfig
¶ Clone a pre-test exciter configuration
Signature
CloneExciterConfig(source)
Parameters: source ( NXOpen.CAE.PreTestExciterConfig
) – Pre-Test exciter configuration to be clonedReturns: Cloned Pre-Test exciter configuration Return type: NXOpen.CAE.PreTestExciterConfig
New in version NX8.0.0.
License requirements: nx_correl_base (“FE Correlation”)
FindObject¶
-
PreTestExciterConfigCollection.
FindObject
¶ Finds a exciter selection configuration with specified name
Signature
FindObject(name)
Parameters: name (str) – exciter selection configuration name to be found Returns: exciter selection configuration found Return type: NXOpen.CAE.PreTestExciterConfig
New in version NX8.0.0.
License requirements: None.
RemoveExciterConfig¶
-
PreTestExciterConfigCollection.
RemoveExciterConfig
¶ Removes and deletes a exciter selection configuration
Signature
RemoveExciterConfig(toRemove)
Parameters: toRemove (int) – Index of the exciter selection configuration to remove New in version NX8.0.0.
License requirements: nx_correl_base (“FE Correlation”)