ResultAccess Class¶
-
class
NXOpen.CAE.
ResultAccess
¶ Bases:
NXOpen.TaggedObject
Represents a specific result state for a given
NXOpen.CAE.Result
.<br/>The result state is defined by
NXOpen.CAE.ResultParameters
<br/>UseNXOpen.CAE.ResultManager
to create anNXOpen.CAE.ResultAccess
.<br/>The unit of result value can be accessed using
NXOpen.CAE.ResultParameters.GetUnit()
An instance of this class can not be obtained
New in version NX6.0.2.
Methods¶
Method | Description |
---|---|
AskCurrentResultDataType | Returns the result type for the current result state defined by NXOpen.CAE.ResultParameters @return |
AskElementEdgeNodalResult | Ask current component value at a specified element, edge and node index. |
AskElementEdgeNodalResultAllComponents | Ask all component values at a specified element index, edge index, node index. |
AskElementEdgeResult | Ask current component value at a specified element and edge index. |
AskElementEdgeResultAllComponents | Ask all component values at a specified element index, edge index. |
AskElementFaceNodalResult | Ask current component value at a specified element, face and node index. |
AskElementFaceNodalResultAllComponents | Ask all component values at a specified element index, face index, node index. |
AskElementFaceResult | Ask current component value at a specified element and face index. |
AskElementFaceResultAllComponents | Ask all component values at a specified element index, face index. |
AskElementNodalResult | Ask element nodal result at a specified element index |
AskElementNodalResultAllComponents | Ask element nodal result at a specified element index Use NXOpen.CAE.ResultAccess.AskResultComponents() to query type of components All values will be returned as a single dimensional array. |
AskElementResult | Ask current component value at a specified element index. |
AskElementResultAllComponents | Ask all component values at a specified element index Use NXOpen.CAE.ResultAccess.AskResultComponents() to query type of components |
AskMaximum | Ask maximum value of current result state defined by NXOpen.CAE.ResultParameters @return |
AskMinMaxLocation | Ask Min and Max value of current result state defined by NXOpen.CAE.ResultParameters If the NXOpen.CAE.ResultLocation is nodal or elemental then ID will be node and element respectively. |
AskMinimum | Ask minimum value of current result state defined by NXOpen.CAE.ResultParameters @return |
AskNMinMaxLocation | Ask for the N extreme Min and Max values and the location of current result state defined by NXOpen.CAE.ResultParameters . |
AskNodalResult | Ask current component value at a specified node index @return |
AskNodalResultAllComponents | Ask all component values at a specified node index Use NXOpen.CAE.ResultAccess.AskResultComponents() to query type of components |
AskResultAtLocation | Ask current component value at a specified location. |
AskResultAtLocationAllComponents | Ask all component values at a specified position. |
AskResultComponents | Return all results components for the current result state defined by NXOpen.CAE.ResultParameters @return |
GetParameters | Returns the NXOpen.CAE.ResultParameters which defines the current result state. |
GetResult | Returns the NXOpen.CAE.Result which defines this result Access object The NXOpen.CAE.Result can be queried in order to set result state in NXOpen.CAE.ResultParameters @return |
IsFullyAveraged | Is result fully averaged @return |
IsResultDefined | Returns true if a result is defined for each node or element index, If the NXOpen.CAE.ResultLocation is Nodal then input indices are expected to be for nodes, for Elemental and ElementNodal the input indices are expected to be for elements @return |
SetParameters | Sets:py:class:NXOpen.CAE.ResultParameters. |
Method Detail¶
AskCurrentResultDataType¶
-
ResultAccess.
AskCurrentResultDataType
¶ Returns the result type for the current result state defined by
NXOpen.CAE.ResultParameters
Signature
AskCurrentResultDataType()
Returns: Return type: NXOpen.CAE.ResultDataType
New in version NX6.0.2.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
AskElementEdgeNodalResult¶
-
ResultAccess.
AskElementEdgeNodalResult
¶ Ask current component value at a specified element, edge and node index.
Edge index will vary from 0 to n-1 where, n is the number of edges on element
Signature
AskElementEdgeNodalResult(elementIndex, edgeIndex, nodeIndex)
Parameters: - elementIndex (int) – element index ranges from 1 to N (where N is number of elements)
NXOpen.CAE.Result.AskNumElements()
- edgeIndex (int) – edge index ranges from 0 to N-1 (where N is number of edges)
NXOpen.CAE.Result.AskNumEdgesOnElement()
- nodeIndex (int) – node index ranges from 1 to N (number of nodes)
NXOpen.CAE.Result.AskNumNodes()
Returns: Return type: float
New in version NX11.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
- elementIndex (int) – element index ranges from 1 to N (where N is number of elements)
AskElementEdgeNodalResultAllComponents¶
-
ResultAccess.
AskElementEdgeNodalResultAllComponents
¶ Ask all component values at a specified element index, edge index, node index.
Edge index will vary from 0 to n-1 where, n is the number of edges on element. Use
NXOpen.CAE.ResultAccess.AskElementEdgeNodalResultAllComponents()
to query all componentsSignature
AskElementEdgeNodalResultAllComponents(elementIndex, edgeIndex, nodeIndex)
Parameters: - elementIndex (int) – element index ranges from 1 to N (where N is number of elements)
NXOpen.CAE.Result.AskNumElements()
- edgeIndex (int) – edge index ranges from 0 to N-1 (whre N is number of edges)
NXOpen.CAE.Result.AskNumEdgesOnElement()
- nodeIndex (int) – node index ranges from 1 to N (number of nodes)
NXOpen.CAE.Result.AskNumNodes()
Returns: Return type: list of float
New in version NX11.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
- elementIndex (int) – element index ranges from 1 to N (where N is number of elements)
AskElementEdgeResult¶
-
ResultAccess.
AskElementEdgeResult
¶ Ask current component value at a specified element and edge index.
Edge index will vary from 0 to n-1 where, n is the number of edges on element.
Signature
AskElementEdgeResult(elementIndex, edgeIndex)
Parameters: - elementIndex (int) – element index ranges from 1 to N (where N is number of elements)
NXOpen.CAE.Result.AskNumElements()
- edgeIndex (int) – edge index ranges from 0 to N-1 (where N is number of edges)
NXOpen.CAE.Result.AskNumEdgesOnElement()
Returns: Return type: float
New in version NX11.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
- elementIndex (int) – element index ranges from 1 to N (where N is number of elements)
AskElementEdgeResultAllComponents¶
-
ResultAccess.
AskElementEdgeResultAllComponents
¶ Ask all component values at a specified element index, edge index.
Edge index will vary from 0 to n-1 where, n is the number of edges on element. Use
NXOpen.CAE.ResultAccess.AskElementFaceResultAllComponents()
to query all componentsSignature
AskElementEdgeResultAllComponents(elementIndex, edgeIndex)
Parameters: - elementIndex (int) – element index ranges from 1 to N (where N is number of elements)
NXOpen.CAE.Result.AskNumElements()
- edgeIndex (int) – edge index ranges from 0 to N-1 (where N is number of edges)
NXOpen.CAE.Result.AskNumEdgesOnElement()
Returns: Return type: list of float
New in version NX11.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
- elementIndex (int) – element index ranges from 1 to N (where N is number of elements)
AskElementFaceNodalResult¶
-
ResultAccess.
AskElementFaceNodalResult
¶ Ask current component value at a specified element, face and node index.
Face index will vary from 0 to n-1 where, n is the number of faces on element.
Signature
AskElementFaceNodalResult(elementIndex, faceIndex, nodeIndex)
Parameters: - elementIndex (int) – element index ranges from 1 to N (where N is number of elements)
NXOpen.CAE.Result.AskNumElements()
- faceIndex (int) – face index ranges from 0 to N-1 (where N is number of faces)
NXOpen.CAE.Result.AskNumFacesOnElement()
- nodeIndex (int) – node index ranges from 1 to N (number of nodes)
NXOpen.CAE.Result.AskNumNodes()
Returns: Return type: float
New in version NX11.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
- elementIndex (int) – element index ranges from 1 to N (where N is number of elements)
AskElementFaceNodalResultAllComponents¶
-
ResultAccess.
AskElementFaceNodalResultAllComponents
¶ Ask all component values at a specified element index, face index, node index.
Face index will vary from 0 to n-1 where, n is the number of faces on element. Use
NXOpen.CAE.ResultAccess.AskElementFaceNodalResultAllComponents()
to all componentsSignature
AskElementFaceNodalResultAllComponents(elementIndex, faceIndex, nodeIndex)
Parameters: - elementIndex (int) – element index ranges from 1 to N (where N is number of elements)
NXOpen.CAE.Result.AskNumElements()
- faceIndex (int) – face index ranges from 0 to N-1 (whre N is number of faces)
NXOpen.CAE.Result.AskNumFacesOnElement()
- nodeIndex (int) – node index ranges from 1 to N (number of nodes)
NXOpen.CAE.Result.AskNumNodes()
Returns: Return type: list of float
New in version NX11.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
- elementIndex (int) – element index ranges from 1 to N (where N is number of elements)
AskElementFaceResult¶
-
ResultAccess.
AskElementFaceResult
¶ Ask current component value at a specified element and face index.
Face index will vary from 0 to n-1 where, n is the number of faces on element.
Signature
AskElementFaceResult(elementIndex, faceIndex)
Parameters: - elementIndex (int) – element index ranges from 1 to N (where N is number of elements)
NXOpen.CAE.Result.AskNumElements()
- faceIndex (int) – face index ranges from 0 to N-1 (where N is number of faces)
NXOpen.CAE.Result.AskNumFacesOnElement()
Returns: Return type: float
New in version NX11.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
- elementIndex (int) – element index ranges from 1 to N (where N is number of elements)
AskElementFaceResultAllComponents¶
-
ResultAccess.
AskElementFaceResultAllComponents
¶ Ask all component values at a specified element index, face index.
Face index will vary from 0 to n-1 where, n is the number of faces on element. Use
NXOpen.CAE.ResultAccess.AskElementFaceResultAllComponents()
to query all componentsSignature
AskElementFaceResultAllComponents(elementIndex, faceIndex)
Parameters: - elementIndex (int) – element index ranges from 1 to N (where N is number of elements)
NXOpen.CAE.Result.AskNumElements()
- faceIndex (int) – face index ranges from 0 to N-1 (where N is number of faces)
NXOpen.CAE.Result.AskNumFacesOnElement()
Returns: Return type: list of float
New in version NX11.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
- elementIndex (int) – element index ranges from 1 to N (where N is number of elements)
AskElementNodalResult¶
-
ResultAccess.
AskElementNodalResult
¶ Overloaded method AskElementNodalResult
AskElementNodalResult(elementIndex)
AskElementNodalResult(elementIndex, nodeIndex)
-------------------------------------
Ask element nodal result at a specified element index
Signature
AskElementNodalResult(elementIndex)
Parameters: elementIndex (int) – Returns: a tuple Return type: A tuple consisting of (nodeLabels, value). nodeLabels is a list of int. index of nodes that forms the element value is a list of float. Values at each node New in version NX6.0.2.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
-------------------------------------
Ask current component value at a specified element index and node index
Signature
AskElementNodalResult(elementIndex, nodeIndex)
Parameters: - elementIndex (int) – element index ranges from 1 to N (where N is number of elements)
NXOpen.CAE.Result.AskNumElements()
- nodeIndex (int) – node index ranges from 1 to N (number of nodes)
NXOpen.CAE.Result.AskNumNodes()
Returns: Return type: float
New in version NX11.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
-------------------------------------
AskElementNodalResultAllComponents¶
-
ResultAccess.
AskElementNodalResultAllComponents
¶ Overloaded method AskElementNodalResultAllComponents
AskElementNodalResultAllComponents(elementIndex)
AskElementNodalResultAllComponents(elementIndex, nodeIndex)
-------------------------------------
Ask element nodal result at a specified element index Use
NXOpen.CAE.ResultAccess.AskResultComponents()
to query type of components All values will be returned as a single dimensional array. The array can be addressed as index = node_index*numComponents + component_indexSignature
AskElementNodalResultAllComponents(elementIndex)
Parameters: elementIndex (int) – Returns: a tuple Return type: A tuple consisting of (nodeIndex, numComponents, value). nodeIndex is a list of int. numComponents is a int. value is a list of float. the array size will be numComponents x totalNodes New in version NX6.0.2.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
-------------------------------------
Ask element nodal result at a specified element index, node index Use
NXOpen.CAE.ResultAccess.AskElementNodalResultAllComponents()
to query all type of componentsSignature
AskElementNodalResultAllComponents(elementIndex, nodeIndex)
Parameters: - elementIndex (int) – element index ranges from 1 to N (where N is number of elements)
NXOpen.CAE.Result.AskNumElements()
- nodeIndex (int) – node index ranges from 1 to N (number of nodes)
NXOpen.CAE.Result.AskNumNodes()
Returns: a tuple
Return type: A tuple consisting of (numComponents, value). numComponents is a int. value is a list of float. the array size will be numComponents x totalNodes
New in version NX11.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
-------------------------------------
AskElementResult¶
-
ResultAccess.
AskElementResult
¶ Overloaded method AskElementResult
AskElementResult(elementIndex)
AskElementResult(elementIndices)
-------------------------------------
Ask current component value at a specified element index.
Signature
AskElementResult(elementIndex)
Parameters: elementIndex (int) – Returns: Return type: float New in version NX6.0.2.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
-------------------------------------
Ask current component value at a specified element indices.
Signature
AskElementResult(elementIndices)
Parameters: elementIndices (list of int) – Returns: Return type: list of float New in version NX8.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
-------------------------------------
AskElementResultAllComponents¶
-
ResultAccess.
AskElementResultAllComponents
¶ Ask all component values at a specified element index Use
NXOpen.CAE.ResultAccess.AskResultComponents()
to query type of componentsSignature
AskElementResultAllComponents(elementIndex)
Parameters: elementIndex (int) – Returns: Return type: list of float New in version NX6.0.2.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
AskMaximum¶
-
ResultAccess.
AskMaximum
¶ Ask maximum value of current result state defined by
NXOpen.CAE.ResultParameters
Signature
AskMaximum()
Returns: Return type: float New in version NX6.0.2.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
AskMinMaxLocation¶
-
ResultAccess.
AskMinMaxLocation
¶ Ask Min and Max value of current result state defined by
NXOpen.CAE.ResultParameters
If theNXOpen.CAE.ResultLocation
is nodal or elemental then ID will be node and element respectively.If it is an element-nodal result then subIDs will be node at which extreme value happens.
Signature
AskMinMaxLocation()
Returns: a tuple Return type: A tuple consisting of (location, min, max, minID, maxID, minSubID, maxSubID). location is a NXOpen.CAE.ResultLocation
. min is a float. max is a float. minID is a int. maxID is a int. minSubID is a int. maxSubID is a int.New in version NX6.0.2.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
AskMinimum¶
-
ResultAccess.
AskMinimum
¶ Ask minimum value of current result state defined by
NXOpen.CAE.ResultParameters
Signature
AskMinimum()
Returns: Return type: float New in version NX6.0.2.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
AskNMinMaxLocation¶
-
ResultAccess.
AskNMinMaxLocation
¶ Ask for the N extreme Min and Max values and the location of current result state defined by
NXOpen.CAE.ResultParameters
.NXOpen.CAE.ResultLocation
will return where the result is defined. If it is an element-nodal result subIDs will be filled with node index and IDs will contain element index. For all other cases subIDs will be 0.Signature
AskNMinMaxLocation(numExtreme)
Parameters: numExtreme (int) – Returns: a tuple Return type: A tuple consisting of (location, min, max, minID, minSubID, maxID, maxSubID). location is a NXOpen.CAE.ResultLocation
. min is a list of float. max is a list of float. minID is a list of int. minSubID is a list of int. maxID is a list of int. maxSubID is a list of int.New in version NX6.0.2.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
AskNodalResult¶
-
ResultAccess.
AskNodalResult
¶ Overloaded method AskNodalResult
AskNodalResult(nodeIndex)
AskNodalResult(nodeIndices)
-------------------------------------
Ask current component value at a specified node index
Signature
AskNodalResult(nodeIndex)
Parameters: nodeIndex (int) – Returns: Return type: float New in version NX6.0.2.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
-------------------------------------
Ask current component value at a specified node indices
Signature
AskNodalResult(nodeIndices)
Parameters: nodeIndices (list of int) – Returns: Return type: list of float New in version NX8.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
-------------------------------------
AskNodalResultAllComponents¶
-
ResultAccess.
AskNodalResultAllComponents
¶ Ask all component values at a specified node index Use
NXOpen.CAE.ResultAccess.AskResultComponents()
to query type of componentsSignature
AskNodalResultAllComponents(nodeIndex)
Parameters: nodeIndex (int) – Returns: Return type: list of float New in version NX6.0.2.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
AskResultAtLocation¶
-
ResultAccess.
AskResultAtLocation
¶ Ask current component value at a specified location.
Only Nodal and Element nodal result will return valid value. If point lies outside model boundary, exception will be thrown. The result value will be interpolated at the given location
Signature
AskResultAtLocation(location)
Parameters: location ( NXOpen.Point3d
) –Returns: Return type: float New in version NX6.0.2.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
AskResultAtLocationAllComponents¶
-
ResultAccess.
AskResultAtLocationAllComponents
¶ Ask all component values at a specified position.
Only Nodal and Element nodal result will return valid value. If point lies outside model boundary, exception will be thrown Use
NXOpen.CAE.ResultAccess.AskResultComponents()
to query type of components. The result value will be interpolated at the given locationSignature
AskResultAtLocationAllComponents(position)
Parameters: position ( NXOpen.Point3d
) –Returns: Return type: list of float New in version NX6.0.2.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
AskResultComponents¶
-
ResultAccess.
AskResultComponents
¶ Return all results components for the current result state defined by
NXOpen.CAE.ResultParameters
Signature
AskResultComponents()
Returns: a tuple Return type: A tuple consisting of (description, components). description is a list of str. components is a list of
NXOpen.CAE.ResultComponent
. .. versionadded:: NX6.0.2License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
GetParameters¶
-
ResultAccess.
GetParameters
¶ Returns the
NXOpen.CAE.ResultParameters
which defines the current result state.<br/>The
NXOpen.CAE.ResultParameters
can be modified but these changes will only take affect afterNXOpen.CAE.ResultAccess.SetParameters()
is called.Signature
GetParameters()
Returns: Return type: NXOpen.CAE.ResultParameters
New in version NX6.0.2.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
GetResult¶
-
ResultAccess.
GetResult
¶ Returns the
NXOpen.CAE.Result
which defines this result Access object TheNXOpen.CAE.Result
can be queried in order to set result state inNXOpen.CAE.ResultParameters
Signature
GetResult()
Returns: Return type: NXOpen.CAE.Result
New in version NX6.0.2.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
IsFullyAveraged¶
-
ResultAccess.
IsFullyAveraged
¶ Is result fully averaged
Signature
IsFullyAveraged()
Returns: Return type: bool New in version NX6.0.2.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
IsResultDefined¶
-
ResultAccess.
IsResultDefined
¶ Overloaded method IsResultDefined
IsResultDefined(indices)
IsResultDefined(entityIndices, subentityIndices)
-------------------------------------
Returns true if a result is defined for each node or element index, If the
NXOpen.CAE.ResultLocation
is Nodal then input indices are expected to be for nodes, for Elemental and ElementNodal the input indices are expected to be for elementsSignature
IsResultDefined(indices)
Parameters: indices (list of int) – Returns: Return type: list of bool New in version NX8.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
-------------------------------------
Returns true if a result is defined for element face/edge or element face/edge nodal result. For Element Face/Edge results entityIndices should be element index and subentityIndices should be face/edge indices. Proper mapping should be maintained in entityIndices and subentityIndices.
Signature
IsResultDefined(entityIndices, subentityIndices)
Parameters: - entityIndices (list of int) – element/node index will vary from 1 to N (where N is number of elements/nodes)
- subentityIndices (list of int) – Face/edge index will vary from 0 to n-1 where, n is the number of faces/edges on element.
Returns: Return type: list of bool
New in version NX11.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
-------------------------------------
SetParameters¶
-
ResultAccess.
SetParameters
¶ Sets:py:class:NXOpen.CAE.ResultParameters.
This will validate any inappropiate settings. If the input is not valid it will revert back to previous settings
Signature
SetParameters(resultParameters)
Parameters: resultParameters ( NXOpen.CAE.ResultParameters
) –New in version NX6.0.2.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)