PostLegendPreference Class¶
-
class
NXOpen.CAE.
PostLegendPreference
¶ Bases:
object
Represents Post-Legend Preferences
To obtain an instance of this class use CAE::CaePost::Preference
New in version NX10.0.0.
Properties¶
Property | Description |
---|---|
Format | Returns or sets the result navigator format |
SignificantPlaces | Returns or sets the result navigator significant places |
Methods¶
Property Detail¶
Format¶
-
PostLegendPreference.
Format
¶ Returns or sets the result navigator format
-------------------------------------
Getter Method
Signature
Format()
Returns: Return type: NXOpen.CAE.PostFormat
New in version NX10.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
-------------------------------------
Setter Method
Signature
Format(format)
Parameters: format ( NXOpen.CAE.PostFormat
) –New in version NX10.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
SignificantPlaces¶
-
PostLegendPreference.
SignificantPlaces
¶ Returns or sets the result navigator significant places
-------------------------------------
Getter Method
Signature
SignificantPlaces()
Returns: Return type: int New in version NX10.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
-------------------------------------
Setter Method
Signature
SignificantPlaces(significantPlaces)
Parameters: significantPlaces (int) – New in version NX10.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)