CaeDOFSet Class¶
-
class
NXOpen.CAE.
CaeDOFSet
¶ Bases:
NXOpen.DisplayableObject
Represents a dofset class
NXOpen.CAE.CaeDOFSet
.To obtain an instance of this object use on of the creator in
NXOpen.CAE.CaeDOFSetCollection
.New in version NX7.5.0.
Properties¶
Property | Description |
---|---|
Color | Returns or sets the color of the object. |
IsBlanked | Returns the blank status of this object. |
IsOccurrence | Returns whether this object is an occurrence or not. |
JournalIdentifier | Returns the identifier that would be recorded in a journal for this object. |
Layer | Returns or sets the layer that the object is in. |
LineFont | Returns or sets the line font of the object. |
LineWidth | Returns or sets the line width of the object. |
Name | Returns the custom name of the object. |
NameLocation | Returns the location of the object’s name. |
OwningComponent | Returns the owning component, if this object is an occurrence. |
OwningPart | Returns the owning part of this object |
Prototype | Returns the prototype of this object if it is an occurrence. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
AddNodes | Add nodes to the CaeDOFSet A true for a dof logical entry would mean that the dof is included for that corresponding node. |
Blank | Blanks the object. |
CreateAttributeIterator | Create an attribute iterator @return A new attribute iterator object |
DeleteAllAttributesByType | Deletes all attributes of a specific type. |
DeleteAttributeByTypeAndTitle | Deletes an attribute by type and title. |
DeleteUserAttribute | Deletes the first attribute encountered with the given Type, Title. |
DeleteUserAttributes | Deletes the attributes on the object, if any, that satisfy the given iterator |
FindObject | Finds the NXOpen.NXObject with the given identifier as recorded in a journal. |
GetAttributeTitlesByType | Gets all the attribute titles of a specific type. |
GetBooleanUserAttribute | Gets a boolean attribute by Title and array Index. |
GetComputationalTimeUserAttribute | Gets a time attribute by Title and array Index. |
GetDisplay | The BC Display object associated with the BC object @return |
GetIntegerAttribute | Gets an integer attribute by title. |
GetIntegerUserAttribute | Gets an integer attribute by Title and array Index. |
GetLabel | Gets the label of the CaeDOFSet @return Label of the DOFSet |
GetNextUserAttribute | Gets the next attribute encountered on the object, if any, that satisfies the given iterator. |
GetNodes | Get the nodes in the DOFSet @return Array of nodes in the DOFSet NXOpen.CAE.FENode |
GetNodesWithDof | Get the nodes with the given dof value in the DOFSet @return Array of nodes NXOpen.CAE.FENode in the DOFSet with the dof value |
GetRealAttribute | Gets a real attribute by title. |
GetRealUserAttribute | Gets a real attribute by Title and array Index. |
GetReferenceAttribute | Gets the reference string (not the calculated value) of a string attribute that uses a reference string. |
GetStringAttribute | Gets a string attribute value by title. |
GetStringUserAttribute | Gets a string attribute by Title and array Index. |
GetTimeAttribute | Gets a time attribute by title. |
GetTimeUserAttribute | Gets a time attribute by Title and array Index. |
GetUserAttribute | Gets the first attribute encountered on the object, if any, with a given Title, Type and array Index. |
GetUserAttributeAsString | Gets the first attribute encountered on the object, if any, with a given title, type and array index. |
GetUserAttributeCount | Gets the count of set attributes on the object, if any, that satisfy the given iterator. |
GetUserAttributeLock | Determine the lock of the given attribute. |
GetUserAttributeSize | Gets the size of the first attribute encountered on the object, if any, with a given Title and Type. |
GetUserAttributeSourceObjects | Returns an array of objects from which this object presents attributes. |
GetUserAttributes | Gets all the attributes that have been set on the given object, if any, that satisfy the given iterator. |
GetUserAttributesAsStrings | Gets all the attributes that have been set on the given object. |
HasUserAttribute | Determines if an attribute exists on the object, that satisfies the given iterator @return |
Highlight | Highlights the object. |
Information | Display information of this DOFSet |
ModifyNodeDofs | Modify the dofs of the passed in nodes in the CaeDOFSet. |
Prints a representation of this object to the system log file. | |
RedisplayObject | Redisplays the object in all views. |
RemoveAllNodes | Remove all nodes from the CaeDOFSet |
RemoveNodes | Remove nodes from the CaeDOFSet. |
RemoveViewDependency | Remove dependency on all views from an object. |
SetAttribute | Creates or modifies an integer attribute. |
SetBooleanUserAttribute | Creates or modifies a boolean attribute with the option to update or not. |
SetLabel | Sets the label of the CaeDOFSet |
SetName | Sets the custom name of the object. |
SetNameLocation | Sets the location of the object’s name. |
SetReferenceAttribute | Creates or modifies a string attribute which uses a reference string. |
SetTimeAttribute | Creates or modifies a time attribute. |
SetTimeUserAttribute | Creates or modifies a time attribute with the option to update or not. |
SetUserAttribute | Creates or modifies an attribute with the option to update or not. |
SetUserAttributeLock | Lock or unlock the given attribute. |
Unblank | Unblanks the object. |
Unhighlight | Unhighlights the object. |
Property Detail¶
IsOccurrence¶
-
CaeDOFSet.
IsOccurrence
¶ Returns whether this object is an occurrence or not.
-------------------------------------
Getter Method
Signature
IsOccurrence()
Returns: This object is an occurrence Return type: bool New in version NX3.0.0.
License requirements: None.
JournalIdentifier¶
-
CaeDOFSet.
JournalIdentifier
¶ Returns the identifier that would be recorded in a journal for this object.
This may not be the same across different releases of the software.
-------------------------------------
Getter Method
Signature
JournalIdentifier()
Returns: Return type: str New in version NX3.0.0.
License requirements: None.
Name¶
-
CaeDOFSet.
Name
¶ Returns the custom name of the object.
-------------------------------------
Getter Method
Signature
Name()
Returns: Return type: str New in version NX3.0.0.
License requirements: None.
OwningComponent¶
-
CaeDOFSet.
OwningComponent
¶ Returns the owning component, if this object is an occurrence.
-------------------------------------
Getter Method
Signature
OwningComponent()
Returns: Return type: NXOpen.Assemblies.Component
New in version NX3.0.0.
License requirements: None.
OwningPart¶
-
CaeDOFSet.
OwningPart
¶ Returns the owning part of this object
-------------------------------------
Getter Method
Signature
OwningPart()
Returns: The owning part of this object or null if it does not have an owner Return type: NXOpen.BasePart
New in version NX3.0.0.
License requirements: None.
Prototype¶
-
CaeDOFSet.
Prototype
¶ Returns the prototype of this object if it is an occurrence.
-------------------------------------
Getter Method
Signature
Prototype()
Returns: The prototype of this object or null if this object is not an occurrence Return type: NXOpen.INXObject
New in version NX3.0.0.
License requirements: None.
Method Detail¶
AddNodes¶
-
CaeDOFSet.
AddNodes
¶ Add nodes to the CaeDOFSet A true for a dof logical entry would mean that the dof is included for that corresponding node.
A false would mean that the dof is not included for that node.
Signature
AddNodes(nodes, dof1, dof2, dof3, dof4, dof5, dof6)
Parameters: - nodes (list of
NXOpen.CAE.FENode
) – Array of nodes to AddNXOpen.CAE.FENode
- dof1 (list of bool) – Array of DOF1 values
- dof2 (list of bool) – Array of DOF2 values
- dof3 (list of bool) – Array of DOF3 values
- dof4 (list of bool) – Array of DOF4 values
- dof5 (list of bool) – Array of DOF5 values
- dof6 (list of bool) – Array of DOF6 values
New in version NX7.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
- nodes (list of
FindObject¶
-
CaeDOFSet.
FindObject
¶ Finds the
NXOpen.NXObject
with the given identifier as recorded in a journal.An object may not return the same value as its JournalIdentifier in different versions of the software. However newer versions of the software should find the same object when FindObject is passed older versions of its journal identifier. In general, this method should not be used in handwritten code and exists to support record and playback of journals.
An exception will be thrown if no object can be found with the given journal identifier.
Signature
FindObject(journalIdentifier)
Parameters: journalIdentifier (str) – Journal identifier of the object Returns: Return type: NXOpen.INXObject
New in version NX3.0.0.
License requirements: None.
GetDisplay¶
-
CaeDOFSet.
GetDisplay
¶ The BC Display object associated with the BC object
Signature
GetDisplay()
Returns: Return type: NXOpen.CAE.CaeDOFSetDisplay
New in version NX7.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
GetLabel¶
-
CaeDOFSet.
GetLabel
¶ Gets the label of the CaeDOFSet
Signature
GetLabel()
Returns: Label of the DOFSet Return type: int New in version NX7.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
GetNodes¶
-
CaeDOFSet.
GetNodes
¶ Get the nodes in the DOFSet
Signature
GetNodes()
Returns: Array of nodes in the DOFSet NXOpen.CAE.FENode
Return type: list of NXOpen.CAE.FENode
New in version NX7.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
GetNodesWithDof¶
-
CaeDOFSet.
GetNodesWithDof
¶ Get the nodes with the given dof value in the DOFSet
Signature
GetNodesWithDof(dof1, dof2, dof3, dof4, dof5, dof6)
Parameters: - dof1 (bool) – DOF1 value
- dof2 (bool) – DOF2 value
- dof3 (bool) – DOF3 value
- dof4 (bool) – DOF4 value
- dof5 (bool) – DOF5 value
- dof6 (bool) – DOF6 value
Returns: Array of nodes
NXOpen.CAE.FENode
in the DOFSet with the dof valueReturn type: list of
NXOpen.CAE.FENode
New in version NX7.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
Information¶
-
CaeDOFSet.
Information
¶ Display information of this DOFSet
Signature
Information()
New in version NX7.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
ModifyNodeDofs¶
-
CaeDOFSet.
ModifyNodeDofs
¶ Modify the dofs of the passed in nodes in the CaeDOFSet.
A true for a dof logical entry would mean that the dof is included for that corresponding node. A false would mean that the dof is not included for that node.
Signature
ModifyNodeDofs(nodes, dof1, dof2, dof3, dof4, dof5, dof6)
Parameters: - nodes (list of
NXOpen.CAE.FENode
) – Array of nodes to modify the dofsNXOpen.CAE.FENode
- dof1 (list of bool) – Array of DOF1 values
- dof2 (list of bool) – Array of DOF2 values
- dof3 (list of bool) – Array of DOF3 values
- dof4 (list of bool) – Array of DOF4 values
- dof5 (list of bool) – Array of DOF5 values
- dof6 (list of bool) – Array of DOF6 values
New in version NX7.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
- nodes (list of
Print¶
-
CaeDOFSet.
Print
¶ Prints a representation of this object to the system log file.
Signature
Print()
New in version NX3.0.0.
License requirements: None.
RemoveAllNodes¶
-
CaeDOFSet.
RemoveAllNodes
¶ Remove all nodes from the CaeDOFSet
Signature
RemoveAllNodes()
New in version NX7.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
RemoveNodes¶
-
CaeDOFSet.
RemoveNodes
¶ Remove nodes from the CaeDOFSet.
If the passed in nodes are not there in the DOF Set, the call does nothing.
Signature
RemoveNodes(nodes)
Parameters: nodes (list of NXOpen.CAE.FENode
) – Array of nodes to RemoveNXOpen.CAE.FENode
New in version NX7.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
SetLabel¶
-
CaeDOFSet.
SetLabel
¶ Sets the label of the CaeDOFSet
Signature
SetLabel(label)
Parameters: label (int) – Label of the DOFSet New in version NX7.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
SetName¶
-
CaeDOFSet.
SetName
¶ Sets the custom name of the object.
NOTE: This method should not be used to edit a read-only object such as a Mirrored PMI object. If it is, the changes will be overridden when the part is updated.
Signature
SetName(name)
Parameters: name (str) – New in version NX3.0.0.
License requirements: None.