CaeDOFSetDisplay Class¶
-
class
NXOpen.CAE.
CaeDOFSetDisplay
¶ Bases:
NXOpen.TaggedObject
Represents a DOF Set display attributes
New in version NX7.5.0.
Properties¶
Property | Description |
---|---|
GraphicSymbolDisplayFlag | Returns or sets the true/false flag based on whether the graphic symbol of the DOF Set is displayed in the graphics window |
NameDisplayFlag | Returns or sets the true/false flag based on whether the name of the DOF Set is displayed in the graphics window |
NodeIdDisplayFlag | Returns or sets the true/false flag based on whether the node id of the DOF Set is displayed in the graphics window |
Scale | Returns or sets the DOF Set display scaling factor this option specifies the scale of the graphic symbol relative to the size of the bounding box of the FE model. |
ShadeGraphicSymbol | Returns or sets the flag indicating whether or not shading of graphic symbols is required |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
UpdateDisplay | Updates the display of the DOF Set |
Property Detail¶
GraphicSymbolDisplayFlag¶
-
CaeDOFSetDisplay.
GraphicSymbolDisplayFlag
¶ Returns or sets the true/false flag based on whether the graphic symbol of the DOF Set is displayed in the graphics window
-------------------------------------
Getter Method
Signature
GraphicSymbolDisplayFlag()
Returns: true when the graphic symbol is displayed, false otherwise Return type: bool New in version NX7.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
-------------------------------------
Setter Method
Signature
GraphicSymbolDisplayFlag(graphicSymbolFlag)
Parameters: graphicSymbolFlag (bool) – true when the graphic symbol should be displayed, false otherwise New in version NX7.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
NameDisplayFlag¶
-
CaeDOFSetDisplay.
NameDisplayFlag
¶ Returns or sets the true/false flag based on whether the name of the DOF Set is displayed in the graphics window
-------------------------------------
Getter Method
Signature
NameDisplayFlag()
Returns: true when the name is displayed, false otherwise Return type: bool New in version NX7.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
-------------------------------------
Setter Method
Signature
NameDisplayFlag(nameFlag)
Parameters: nameFlag (bool) – true when the name should be displayed, false otherwise New in version NX7.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
NodeIdDisplayFlag¶
-
CaeDOFSetDisplay.
NodeIdDisplayFlag
¶ Returns or sets the true/false flag based on whether the node id of the DOF Set is displayed in the graphics window
-------------------------------------
Getter Method
Signature
NodeIdDisplayFlag()
Returns: true when the node id is displayed, false otherwise Return type: bool New in version NX7.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
-------------------------------------
Setter Method
Signature
NodeIdDisplayFlag(nodeIdFlag)
Parameters: nodeIdFlag (bool) – true when the node id should be displayed, false otherwise New in version NX7.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
Scale¶
-
CaeDOFSetDisplay.
Scale
¶ Returns or sets the DOF Set display scaling factor this option specifies the scale of the graphic symbol relative to the size of the bounding box of the FE model.
-------------------------------------
Getter Method
Signature
Scale()
Returns: 1 is the smallest - 100 is the largest Return type: int New in version NX7.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
-------------------------------------
Setter Method
Signature
Scale(scale)
Parameters: scale (int) – 1 is the smallest - 100 is the largest New in version NX7.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
ShadeGraphicSymbol¶
-
CaeDOFSetDisplay.
ShadeGraphicSymbol
¶ Returns or sets the flag indicating whether or not shading of graphic symbols is required
-------------------------------------
Getter Method
Signature
ShadeGraphicSymbol()
Returns: true when shading is required, false otherwise Return type: bool New in version NX7.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
-------------------------------------
Setter Method
Signature
ShadeGraphicSymbol(shadeGsymbolFlag)
Parameters: shadeGsymbolFlag (bool) – true when shading is required, false otherwise New in version NX7.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)