CfdAutoRefinementConstraintBuilder Class¶
-
class
NXOpen.CAE.
CfdAutoRefinementConstraintBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.CAE.CfdAutoRefinementConstraint
builderTo create a new instance of this class, use
NXOpen.CAE.CfdAutoRefinementConstraintCollection.CreateBuilder()
New in version NX11.0.0.
Properties¶
Property | Description |
---|---|
LocalResolution | Returns the minimum local resolution |
LocalSubdivision | Returns or sets the maximum local subdivision |
NameString | Returns or sets the name of the constraint |
PriorityLevel | Returns or sets the priority level |
SelectObject | Returns the list of selected objects |
SizingOption | Returns or sets the sizing option |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
CfdAutoRefinementConstraintBuilderLocalSubdivisions Enumeration | The maximum local subdivision |
CfdAutoRefinementConstraintBuilderPriority Enumeration | The priority level |
CfdAutoRefinementConstraintBuilderSizing Enumeration | The sizing option |
Property Detail¶
LocalResolution¶
-
CfdAutoRefinementConstraintBuilder.
LocalResolution
¶ Returns the minimum local resolution
-------------------------------------
Getter Method
Signature
LocalResolution()
Returns: Return type: NXOpen.Expression
New in version NX11.0.0.
License requirements: None.
LocalSubdivision¶
-
CfdAutoRefinementConstraintBuilder.
LocalSubdivision
¶ Returns or sets the maximum local subdivision
-------------------------------------
Getter Method
Signature
LocalSubdivision()
Returns: Return type: NXOpen.CAE.CfdAutoRefinementConstraintBuilderLocalSubdivisions
New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
LocalSubdivision(localSubdivision)
Parameters: localSubdivision ( NXOpen.CAE.CfdAutoRefinementConstraintBuilderLocalSubdivisions
) –New in version NX11.0.0.
License requirements: nx_adv_fluid_mod (“NX Advanced Fluid Modeling”)
NameString¶
-
CfdAutoRefinementConstraintBuilder.
NameString
¶ Returns or sets the name of the constraint
-------------------------------------
Getter Method
Signature
NameString()
Returns: Return type: str New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
NameString(nameString)
Parameters: nameString (str) – New in version NX11.0.0.
License requirements: nx_adv_fluid_mod (“NX Advanced Fluid Modeling”)
PriorityLevel¶
-
CfdAutoRefinementConstraintBuilder.
PriorityLevel
¶ Returns or sets the priority level
-------------------------------------
Getter Method
Signature
PriorityLevel()
Returns: Return type: NXOpen.CAE.CfdAutoRefinementConstraintBuilderPriority
New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PriorityLevel(priorityLevel)
Parameters: priorityLevel ( NXOpen.CAE.CfdAutoRefinementConstraintBuilderPriority
) –New in version NX11.0.0.
License requirements: nx_adv_fluid_mod (“NX Advanced Fluid Modeling”)
SelectObject¶
-
CfdAutoRefinementConstraintBuilder.
SelectObject
¶ Returns the list of selected objects
-------------------------------------
Getter Method
Signature
SelectObject()
Returns: Return type: NXOpen.SelectDisplayableObjectList
New in version NX11.0.0.
License requirements: None.
SizingOption¶
-
CfdAutoRefinementConstraintBuilder.
SizingOption
¶ Returns or sets the sizing option
-------------------------------------
Getter Method
Signature
SizingOption()
Returns: Return type: NXOpen.CAE.CfdAutoRefinementConstraintBuilderSizing
New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SizingOption(sizingOption)
Parameters: sizingOption ( NXOpen.CAE.CfdAutoRefinementConstraintBuilderSizing
) –New in version NX11.0.0.
License requirements: nx_adv_fluid_mod (“NX Advanced Fluid Modeling”)
Method Detail¶
Validate¶
-
CfdAutoRefinementConstraintBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.