DurabilityEventStrengthSettingsBuilderOrthotropicFailureCriterionEnum Enumeration

NXOpen.CAE.DurabilityEventStrengthSettingsBuilder.OrthotropicFailureCriterionEnum is an alias for NXOpen.CAE.DurabilityEventStrengthSettingsBuilderOrthotropicFailureCriterionEnum

class NXOpen.CAE.DurabilityEventStrengthSettingsBuilderOrthotropicFailureCriterionEnum

Bases: object

the orthotropic Failure criterion enum.

Enum Members

Enum Member Enum Member Description
Hill
Hill
Hoffman
Hoffman
TsaiWu
Tsai-Wu
MaximumStress
Maximum Stress
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.