ElementProjectBuilderElementDimensionType Enumeration¶
NXOpen.CAE.ElementProjectBuilder.ElementDimensionType is an alias for NXOpen.CAE.ElementProjectBuilderElementDimensionType
-
class
NXOpen.CAE.
ElementProjectBuilderElementDimensionType
¶ Bases:
object
Dimension of element to be projected
Enum Members
Enum Member Enum Member Description Any beam and/or shell elementBeam beam elementShell shell element-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-