ReassignElementsBuilderElementTypeOption Enumeration¶
NXOpen.CAE.ReassignElementsBuilder.ElementTypeOption is an alias for NXOpen.CAE.ReassignElementsBuilderElementTypeOption
-
class
NXOpen.CAE.
ReassignElementsBuilderElementTypeOption
¶ Bases:
object
Indicates the element types for each dimension.
Since this varies dynamically based on the language and dimension Will not touch this for now.
Enum Members
Enum Member Enum Member Description FirstValue -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-