LaminateSpreadsheetReportBuilderSortingType Enumeration¶
NXOpen.CAE.LaminateSpreadsheetReportBuilder.SortingType is an alias for NXOpen.CAE.LaminateSpreadsheetReportBuilderSortingType
-
class
NXOpen.CAE.
LaminateSpreadsheetReportBuilderSortingType
¶ Bases:
object
Sorting rule for the spreadsheet post report
Enum Members
Enum Member Enum Member Description ElementId Sort results using the element idPlyId Sort results using the ply idStressXX Sort results using the stress XX componentStressYY Sort results using the stress YY componentStressZZ Sort results using the stress ZZ componentStressXY Sort results using the stress XY componentStressZX Sort results using the stress ZX componentStressYZ Sort results using the stress YZ componentStressMaxP Sort results using the maximum principal stressStressMinP Sort results using the minimum principal stressStressMaxS Sort results using the maximum shear stressStrainXX Sort results using the strain XX componentStrainYY Sort results using the strain XX componentStrainZZ Sort results using the strain XX componentStrainXY Sort results using the strain XX componentStrainZX Sort results using the strain XX componentStrainYZ Sort results using the strain XX componentStrainMaxP Sort results using the maximum principal strainStrainMinP Sort results using the minimum principal strainStrainMaxS Sort results using the maximum shear strainPlyFailureIndex Sort results based on the ply failure indexPlyStrengthRatio Sort results based on the ply strength ratioPlyMarginofSafety Sort results based on the ply margin of safetyBondFailureIndex Sort results based on the bonding failure indexBondStrengthRatio Sort results based on the bonding strength ratioBondMarginofSafety Sort results based on the bonding margin of safety-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-