WeldBuilderNumberOfPointsOnEdgeType Enumeration

NXOpen.CAE.WeldBuilder.NumberOfPointsOnEdgeType is an alias for NXOpen.CAE.WeldBuilderNumberOfPointsOnEdgeType

class NXOpen.CAE.WeldBuilderNumberOfPointsOnEdgeType

Bases: object

Represents the options for specifying maximum number of weld points on an edge

Enum Members

Enum Member Enum Member Description
MaximumNumber
Create the maximum number of points on an edge
SpecifiedNumber
Specify the number of points to be created on an edge
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.