PreTestSolutionCollection Class

class NXOpen.CAE.PreTestSolutionCollection

Bases: object

Represents a collection of pre-test setups

To obtain an instance of this class, refer to NXOpen.CAE.CorrelManager

New in version NX7.5.0.

Properties

Property Description
ActivePretest Returns or sets the active pre-test

Methods

Method Description
ClonePretest Clone a pre-test @return Cloned Pre-Test
CreateAutoMacViewerBuilder Creates an AutoMAC results display builder @return AutoMac Builder.
CreateExciterConfigBuilder Creates a exciter configuration dialog builder @return Exciter Configuration Builder.
CreatePretestBuilder Creates a pre-test dialog builder @return Pre-Test Builder
CreatePretestDofsetBuilder Creates a dof set dialog builder @return Dof Set Builder.
CreateSensorConfigBuilder Creates a sensor configuration dialog builder @return Sensor Configuration Builder.
DeletePretest Delete a pre-test
FindObject Finds a pre-test setup with specified name @return Pre-Test found

Property Detail

ActivePretest

PreTestSolutionCollection.ActivePretest

Returns or sets the active pre-test

-------------------------------------

Getter Method

Signature ActivePretest()

Returns:Active Pre-Test
Return type:NXOpen.CAE.PreTestSolution

New in version NX7.5.0.

License requirements: None.

-------------------------------------

Setter Method

Signature ActivePretest(pretest)

Parameters:pretest (NXOpen.CAE.PreTestSolution) – Pre-Test to be set active

New in version NX7.5.0.

License requirements: nx_correl_base (“FE Correlation”)

Method Detail

ClonePretest

PreTestSolutionCollection.ClonePretest

Clone a pre-test

Signature ClonePretest(source)

Parameters:source (NXOpen.CAE.PreTestSolution) – Pre-Test to be cloned
Returns:Cloned Pre-Test
Return type:NXOpen.CAE.PreTestSolution

New in version NX7.5.0.

License requirements: nx_correl_base (“FE Correlation”)

CreateAutoMacViewerBuilder

PreTestSolutionCollection.CreateAutoMacViewerBuilder

Creates an AutoMAC results display builder

Signature CreateAutoMacViewerBuilder(macInput)

Parameters:macInput (NXOpen.TaggedObject) – Mac Input.
Returns:AutoMac Builder.
Return type:NXOpen.CAE.AutoMacViewerBuilder

New in version NX7.5.0.

License requirements: nx_correl_base (“FE Correlation”)

CreateExciterConfigBuilder

PreTestSolutionCollection.CreateExciterConfigBuilder

Creates a exciter configuration dialog builder

Signature CreateExciterConfigBuilder(exciterConfig)

Parameters:exciterConfig (NXOpen.CAE.PreTestExciterConfig) – Exciter Configuration being edited.
Returns:Exciter Configuration Builder.
Return type:NXOpen.CAE.PreTestExciterConfigBuilder

New in version NX8.0.0.

License requirements: nx_correl_base (“FE Correlation”)

CreatePretestBuilder

PreTestSolutionCollection.CreatePretestBuilder

Creates a pre-test dialog builder

Signature CreatePretestBuilder(pretest)

Parameters:pretest (NXOpen.CAE.PreTestSolution) – Edited Pre-Test. Can be NULL if creating a new Pre-Test.
Returns:Pre-Test Builder
Return type:NXOpen.CAE.PreTestSolutionBuilder

New in version NX7.5.0.

License requirements: nx_correl_base (“FE Correlation”)

CreatePretestDofsetBuilder

PreTestSolutionCollection.CreatePretestDofsetBuilder

Creates a dof set dialog builder

Signature CreatePretestDofsetBuilder(dofset)

Parameters:dofset (NXOpen.CAE.PreTestDofSet) – Dof Set being edited.
Returns:Dof Set Builder.
Return type:NXOpen.CAE.PreTestDofSetBuilder

New in version NX7.5.0.

License requirements: nx_correl_base (“FE Correlation”)

CreateSensorConfigBuilder

PreTestSolutionCollection.CreateSensorConfigBuilder

Creates a sensor configuration dialog builder

Signature CreateSensorConfigBuilder(sensorConfig)

Parameters:sensorConfig (NXOpen.CAE.PreTestSensorConfig) – Sensor Configuration being edited.
Returns:Sensor Configuration Builder.
Return type:NXOpen.CAE.PreTestSensorConfigBuilder

New in version NX7.5.0.

License requirements: nx_correl_base (“FE Correlation”)

DeletePretest

PreTestSolutionCollection.DeletePretest

Delete a pre-test

Signature DeletePretest(pretest)

Parameters:pretest (NXOpen.CAE.PreTestSolution) – Pre-Test to be deleted

New in version NX7.5.0.

License requirements: nx_correl_base (“FE Correlation”)

FindObject

PreTestSolutionCollection.FindObject

Finds a pre-test setup with specified name

Signature FindObject(name)

Parameters:name (str) – Pre-Test name to be found
Returns:Pre-Test found
Return type:NXOpen.CAE.PreTestSolution

New in version NX7.5.0.

License requirements: None.