SolidPropertyCheckBuilderUserUnit Enumeration

NXOpen.CAE.SolidPropertyCheckBuilder.UserUnit is an alias for NXOpen.CAE.SolidPropertyCheckBuilderUserUnit

class NXOpen.CAE.SolidPropertyCheckBuilderUserUnit

Bases: object

User Specified output unit

Enum Members

Enum Member Enum Member Description
DefaultUnit
Load unit = same as system default unit
KgMilli
mass = kg, cg = mm, volume = mm^3 mmoi = kg-mm^2
LbmIn
mass = lbm, cg = in, volume = in^3 mmoi = lbm-in^2
LbfInSec
mass = lbf-sec^2/in, cg = in, volume = in^3 mmoi = lbf-in-sec^2
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.