SimLoadGroup Class¶
-
class
NXOpen.CAE.
SimLoadGroup
¶ Bases:
NXOpen.CAE.SimBcGroup
Represents a load group in a solution or solution step
Not support KF.
New in version NX9.0.0.
Properties¶
Property | Description |
---|---|
GroupContainer | Returns the solution or solution step owning this BC group |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Add | Adds a load to this group |
AddLoadSet | Adds a load set to this group |
GetLoadSets | Gets the load sets in this group @return the load sets in this group |
GetLoads | Gets the loads in this group @return the loads in this group |
Remove | Removes a load from this group |
RemoveAll | Removes all loads from this group |
RemoveAllLoadSets | Remove all load sets from this group |
RemoveLoadSet | Removes a load from this group |
SetBoltLoadSequence | Set the bolt load sequence |
Method Detail¶
Add¶
-
SimLoadGroup.
Add
¶ Adds a load to this group
Signature
Add(tLoad)
Parameters: tLoad ( NXOpen.CAE.SimLoad
) – the load to be addedNew in version NX9.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
AddLoadSet¶
-
SimLoadGroup.
AddLoadSet
¶ Adds a load set to this group
Signature
AddLoadSet(tLoadSet)
Parameters: tLoadSet ( NXOpen.CAE.SimLoadSet
) – the load to be addedNew in version NX10.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
GetLoadSets¶
-
SimLoadGroup.
GetLoadSets
¶ Gets the load sets in this group
Signature
GetLoadSets()
Returns: the load sets in this group Return type: list of NXOpen.CAE.SimLoadSet
New in version NX10.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
GetLoads¶
-
SimLoadGroup.
GetLoads
¶ Gets the loads in this group
Signature
GetLoads()
Returns: the loads in this group Return type: list of NXOpen.CAE.SimLoad
New in version NX9.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
Remove¶
-
SimLoadGroup.
Remove
¶ Removes a load from this group
Signature
Remove(tLoad)
Parameters: tLoad ( NXOpen.CAE.SimLoad
) – the load to be removedNew in version NX9.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
RemoveAll¶
-
SimLoadGroup.
RemoveAll
¶ Removes all loads from this group
Signature
RemoveAll()
New in version NX9.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
RemoveAllLoadSets¶
-
SimLoadGroup.
RemoveAllLoadSets
¶ Remove all load sets from this group
Signature
RemoveAllLoadSets()
New in version NX10.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
RemoveLoadSet¶
-
SimLoadGroup.
RemoveLoadSet
¶ Removes a load from this group
Signature
RemoveLoadSet(tLoadSet)
Parameters: tLoadSet ( NXOpen.CAE.SimLoadSet
) – the load to be removedNew in version NX10.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)