PrimitiveRecipeMeshBuilderType Enumeration¶
NXOpen.CAE.PrimitiveRecipeMeshBuilder.Type is an alias for NXOpen.CAE.PrimitiveRecipeMeshBuilderType
-
class
NXOpen.CAE.
PrimitiveRecipeMeshBuilderType
¶ Bases:
object
Mesh primitive type
Enum Members
Enum Member Enum Member Description Sphere Sphere PrimitivePlane Plane PrimitivePointSet Point Set PrimitiveIsoPower ISO Power (ISO3744) PrimitiveBoxSurface Box Surface PrimitiveBoxSolid Box Solid PrimitiveCircle Circle PrimitiveLine Line Primitive-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-