DependentMeshBuilderMeshType Enumeration

NXOpen.CAE.DependentMeshBuilder.MeshType is an alias for NXOpen.CAE.DependentMeshBuilderMeshType

class NXOpen.CAE.DependentMeshBuilderMeshType

Bases: object

The mesh type for face dependency

Enum Members

Enum Member Enum Member Description
Free
Free mesh
Map
Map mesh
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.