GroupElemMethodElemOptionElemOption Enumeration

NXOpen.CAE.GroupElemMethodElemOption.ElemOption is an alias for NXOpen.CAE.GroupElemMethodElemOptionElemOption

class NXOpen.CAE.GroupElemMethodElemOptionElemOption

Bases: object

Used to specify the sub type of selected objects e.

g face of an element, edge of an element ..etc

Enum Members

Enum Member Enum Member Description
ElemAll
return all elements in the group
Elem0d
return 0D elements in the group
Elem1d
return 1D elements in the group
Elem2d
return 2D elements in the group
Elem3d
return 3D elements in the group
Elemface2d
return 2D elements in the group as element faces
Elemedge1d
return 1D elements in the group as element edges
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.