ElementTranslateBuilderElemDimensionType Enumeration¶
NXOpen.CAE.ElementTranslateBuilder.ElemDimensionType is an alias for NXOpen.CAE.ElementTranslateBuilderElemDimensionType
-
class
NXOpen.CAE.
ElementTranslateBuilderElemDimensionType
¶ Bases:
object
Dimension of the elements to be created
Enum Members
Enum Member Enum Member Description Any any element can be selectedBeam only beam elements can be selectedShell only shell elements can be selectedSolid only solid elements can be selected-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-