CaeSession Class¶
-
class
NXOpen.CAE.
CaeSession
¶ Bases:
object
This class provides access to all session related CAE functionality
To obtain an instance of this class, refer to
NXOpen.Session
New in version NX7.5.0.
“MaterialUtils”, ” Returns the <ja_class>NXOpen.MaterialUtilities</ja_class> instance belonging to this session ” “AssociationUtils”, ” Returns the <ja_class>NXOpen.CAE.AssociationUtilities</ja_class> instance belonging to this session “
Methods¶
Method | Description |
---|---|
GetDataContainer | Returns a NXOpen.CAE.CaeDataContainer to be used for specifying input parameters operations like Simulation Import and Export. |
ImportSimulation | Creates a NXOpen.CAE.SimPart and a NXOpen.CAE.FemPart from solver specific data. |
MaterialUtils¶
-
CaeSession.
MaterialUtils
¶ Returns the
NXOpen.MaterialUtilities
instance belonging to this sessionSignature
MaterialUtils()
New in version NX10.0.0.
Returns: Return type: NXOpen.MaterialUtilities
AssociationUtils¶
-
CaeSession.
AssociationUtils
¶ Returns the
NXOpen.CAE.AssociationUtilities
instance belonging to this sessionSignature
AssociationUtils()
New in version NX11.0.0.
Returns: Return type: NXOpen.CAE.AssociationUtilities
Method Detail¶
GetDataContainer¶
-
CaeSession.
GetDataContainer
¶ Returns a
NXOpen.CAE.CaeDataContainer
to be used for specifying input parameters operations like Simulation Import and Export.Signature
GetDataContainer()
Returns: the Cae Data Container Return type: NXOpen.CAE.CaeDataContainer
New in version NX7.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
ImportSimulation¶
-
CaeSession.
ImportSimulation
¶ Creates a
NXOpen.CAE.SimPart
and aNXOpen.CAE.FemPart
from solver specific data.Import is driven by that properties defined in the input
NXOpen.CAE.CaeDataContainer
propertyList. The exact properties can vary from solver to solver.Signature
ImportSimulation(solverName, propertyList)
Parameters: - solverName (str) – the solver name to indicate what type of data is being imported
- propertyList (
NXOpen.CAE.CaeDataContainer
) – the import parameters seeGetDataContainer()
.
Returns: Return type: New in version NX7.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)