PreTestSolutionBuilderModeConversionType Enumeration

NXOpen.CAE.PreTestSolutionBuilder.ModeConversionType is an alias for NXOpen.CAE.PreTestSolutionBuilderModeConversionType

class NXOpen.CAE.PreTestSolutionBuilderModeConversionType

Bases: object

Enum type for the complex mode conversion settings

Enum Members

Enum Member Enum Member Description
SignedAmplitude
No triax sensors required
ComplexTransform
All sensors must be triax
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.