DurabilityDamageEvaluationBuilderProbabilityOptionEnum Enumeration

NXOpen.CAE.DurabilityDamageEvaluationBuilder.ProbabilityOptionEnum is an alias for NXOpen.CAE.DurabilityDamageEvaluationBuilderProbabilityOptionEnum

class NXOpen.CAE.DurabilityDamageEvaluationBuilderProbabilityOptionEnum

Bases: object

the Probability Option.

Enum Members

Enum Member Enum Member Description
NumberOfStandardDeviations
Number of Std. Dev.
ProbabilityOfFailure
Prob. Of Failure
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.