LocalRemeshBuilder Class¶
-
class
NXOpen.CAE.
LocalRemeshBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.CAE.LocalRemeshBuilder
To create a new instance of this class, use
NXOpen.CAE.MeshManager.CreateLocalRemeshBuilder()
Default values.
Property Value FactorValue.Value 0.5 SizeOption Factor SizeValue.Value 1.0 Transition 50 New in version NX7.5.2.
Properties¶
Property | Description |
---|---|
ElementList | Returns the select elements |
FactorValue | Returns the factor value |
SizeOption | Returns or sets the size option |
SizeValue | Returns the size value |
Tag | Returns the Tag for this object. |
Transition | Returns or sets the transition |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
LocalRemeshBuilderOption Enumeration | Size Option |
Property Detail¶
ElementList¶
-
LocalRemeshBuilder.
ElementList
¶ Returns the select elements
-------------------------------------
Getter Method
Signature
ElementList()
Returns: Return type: NXOpen.CAE.SelectElementsBuilder
New in version NX7.5.2.
License requirements: None.
FactorValue¶
-
LocalRemeshBuilder.
FactorValue
¶ Returns the factor value
-------------------------------------
Getter Method
Signature
FactorValue()
Returns: Return type: NXOpen.Expression
New in version NX7.5.2.
License requirements: None.
SizeOption¶
-
LocalRemeshBuilder.
SizeOption
¶ Returns or sets the size option
-------------------------------------
Getter Method
Signature
SizeOption()
Returns: Return type: NXOpen.CAE.LocalRemeshBuilderOption
New in version NX7.5.2.
License requirements: None.
-------------------------------------
Setter Method
Signature
SizeOption(sizeOption)
Parameters: sizeOption ( NXOpen.CAE.LocalRemeshBuilderOption
) –New in version NX7.5.2.
License requirements: nx_masterfem (“Finite Element Modeling”)
SizeValue¶
-
LocalRemeshBuilder.
SizeValue
¶ Returns the size value
-------------------------------------
Getter Method
Signature
SizeValue()
Returns: Return type: NXOpen.Expression
New in version NX7.5.2.
License requirements: None.
Transition¶
-
LocalRemeshBuilder.
Transition
¶ Returns or sets the transition
-------------------------------------
Getter Method
Signature
Transition()
Returns: Return type: int New in version NX7.5.2.
License requirements: None.
-------------------------------------
Setter Method
Signature
Transition(transition)
Parameters: transition (int) – New in version NX7.5.2.
License requirements: nx_masterfem (“Finite Element Modeling”)
Method Detail¶
Validate¶
-
LocalRemeshBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.