DurabilityEventSolverBuilderSubmitOptionsEnum Enumeration

NXOpen.CAE.DurabilityEventSolverBuilder.SubmitOptionsEnum is an alias for NXOpen.CAE.DurabilityEventSolverBuilderSubmitOptionsEnum

class NXOpen.CAE.DurabilityEventSolverBuilderSubmitOptionsEnum

Bases: object

the submit options enum.

Enum Members

Enum Member Enum Member Description
Solve
Solve
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.