SimLoadRecipeMapEntryTargetTypesTargetTypes Enumeration¶
NXOpen.CAE.SimLoadRecipeMapEntryTargetTypes.TargetTypes is an alias for NXOpen.CAE.SimLoadRecipeMapEntryTargetTypesTargetTypes
-
class
NXOpen.CAE.
SimLoadRecipeMapEntryTargetTypesTargetTypes
¶ Bases:
object
This enum defines the target type options of a
NXOpen.CAE.SimLoadRecipeMapEntry
Enum Members
.
- . csv-table::
header: “Enum Member”, “Enum Member Description” “Unknown”, ” Unkown target type ” “Node”, ” Node ” “NodeGroup”, ” Nodes in a group. ” “NodeMesh”, ” Nodes in a mesh. ” “Face”, ” Element face ” “FaceGroup”, ” Element faces in a group. ” “FaceMesh”, ” Element faces in a mesh. ” “NodeFem”, ” Nodes in a fem model. ” “FaceFem”, ” Element faces in a fem model. “
-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.