MeshDisplaySettings Class¶
-
class
NXOpen.CAE.
MeshDisplaySettings
¶ Bases:
NXOpen.TransientObject
Represents the base MeshDisplaySettings class for Mesh class
This is an abstract class, and cannot be created.
New in version NX5.0.0.
Methods¶
Method | Description |
---|---|
Dispose | Frees the object from memory. |
UseCustomerDefaultsDisplaySettings | Use display settings from the Customer Defaults. |
UseMeshCollectorDisplaySettings | Use display settings from the Mesh Collector. |
Property Detail¶
Color¶
-
MeshDisplaySettings.
Color
¶ Returns or sets the element color.
-------------------------------------
Getter Method
Signature
Color()
Returns: Return type: Id New in version NX8.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
-------------------------------------
Setter Method
Signature
Color(color)
Parameters: color (Id) – New in version NX8.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
Method Detail¶
Dispose¶
-
MeshDisplaySettings.
Dispose
¶ Frees the object from memory.
After this method is called, it is illegal to use the object. In .NET, this method is automatically called when the object is deleted by the garbage collector.
Signature
Dispose()
New in version NX8.5.0.
License requirements: None.
UseCustomerDefaultsDisplaySettings¶
-
MeshDisplaySettings.
UseCustomerDefaultsDisplaySettings
¶ Use display settings from the Customer Defaults.
Signature
UseCustomerDefaultsDisplaySettings()
New in version NX8.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
UseMeshCollectorDisplaySettings¶
-
MeshDisplaySettings.
UseMeshCollectorDisplaySettings
¶ Use display settings from the Mesh Collector.
Signature
UseMeshCollectorDisplaySettings()
New in version NX8.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)