DurabilityStaticEventBuilder Class

class NXOpen.CAE.DurabilityStaticEventBuilder

Bases: NXOpen.CAE.DurabilityEventBuilder

Represents the builder for the static durability event.

There is no kf creator for this.

New in version NX7.5.0.

Properties

Property Description
EventName Returns or sets the event name.
ExcitationType Returns or sets the excitation type.
ResultSourceTag Returns or sets the source of results for the event.
Tag Returns the Tag for this object.

Methods

Method Description
Commit Commits any edits that have been applied to the builder.
Destroy Deletes the builder, and cleans up any objects created by the builder.
GetCommittedObjects For builders that create more than one object, this method returns the objects that are created by commit.
GetObject Returns the object currently being edited by this builder.
SetAxissearch The stress axes stored inside the event.
SetFatigue The event fatigue settings stored inside the event.
SetSolveoptions The event overrides.
SetStrength The event strength settings stored inside the event.
ShowResults Updates the model to reflect the result of an edit to the model for all builders that support showing results.
Validate Validate whether the inputs to the component are sufficient for commit to be called.

Enumerations

DurabilityStaticEventBuilderExcitationTypeEnum Enumeration the static excitation type.

Property Detail

ExcitationType

DurabilityStaticEventBuilder.ExcitationType

Returns or sets the excitation type.

-------------------------------------

Getter Method

Signature ExcitationType()

Returns:
Return type:NXOpen.CAE.DurabilityStaticEventBuilderExcitationTypeEnum

New in version NX7.5.0.

License requirements: nx_adv_durability (“NX Advanced Durability”)

-------------------------------------

Setter Method

Signature ExcitationType(excitationType)

Parameters:excitationType (NXOpen.CAE.DurabilityStaticEventBuilderExcitationTypeEnum) –

New in version NX7.5.0.

License requirements: nx_adv_durability (“NX Advanced Durability”)

Method Detail

Validate

DurabilityStaticEventBuilder.Validate

Validate whether the inputs to the component are sufficient for commit to be called.

If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.

Signature Validate()

Returns:Was self validation successful
Return type:bool

New in version NX3.0.1.

License requirements: None.