PostAnnotationBuilder Class¶
-
class
NXOpen.CAE.
PostAnnotationBuilder
¶ Bases:
NXOpen.TransientObject
Builder to create
NXOpen.CAE.PostAnnotation
fromNXOpen.CAE.Post
<br/>User can pass entities which are same as current postview location.
The entities have to be passed in following manner
- Elemental Result - Use
NXOpen.CAE.PostAnnotationBuilder.SetElements()
only. - Nodal Result - Use
NXOpen.CAE.PostAnnotationBuilder.SetNodes()
only. - Element-Nodal Result - Use
NXOpen.CAE.PostAnnotationBuilder.SetElements()
andNXOpen.CAE.PostAnnotationBuilder.SetNodes()
.
- Number of entities should be same for both.
- Element-Face Result - Use
NXOpen.CAE.PostAnnotationBuilder.SetElements()
andNXOpen.CAE.PostAnnotationBuilder.SetEdgeFace()
.
- Element-Face Result - Use
- Number of entities should be same for both.
- Element-Edge Result - Use
NXOpen.CAE.PostAnnotationBuilder.SetElements()
andNXOpen.CAE.PostAnnotationBuilder.SetEdgeFace()
.
- Element-Edge Result - Use
- Number of entities should be same for both.
- Element-Face-Node Result - Use
NXOpen.CAE.PostAnnotationBuilder.SetElements()
,NXOpen.CAE.PostAnnotationBuilder.SetNodes()
- Element-Face-Node Result - Use
- and
NXOpen.CAE.PostAnnotationBuilder.SetEdgeFace()
. Number of entities should be same for all three. - Element-Edge-Node Result - Use
NXOpen.CAE.PostAnnotationBuilder.SetElements()
,NXOpen.CAE.PostAnnotationBuilder.SetNodes()
- Element-Edge-Node Result - Use
and
NXOpen.CAE.PostAnnotationBuilder.SetEdgeFace()
. Number of entities should be same for all three.<br/>Though entities are being passed separately, they work as a set, so no of entities must be same for all. <br/> <li>Cylic-Symmetric Result</li> Number of Sectors should be same as Number of entities <li>Axis-Symmetric Result</li> Number of Angles should be same as number of entities.
To obtain an instance of this class use CAE::Post
New in version NX11.0.0.
- Elemental Result - Use
Methods¶
Method | Description |
---|---|
CommitAnnotation | Commits the annotation to create annotation object @return |
Delete | Deletes the annotation builder. |
Dispose | Frees the object from memory. |
SetAnnotationType | Set the annotation type |
SetCoordinate | Set the coordinates for user annotation |
SetEdgeFace | Set the edge or face id for which annotation is defined |
SetElements | Set the element ids for which annotation is defined |
SetName | Set the annotation name |
SetNodes | Set the node ids for which annotation is defined |
SetNumMinMax | Set the number of min/max annotation for min/max type of annotation |
SetSectionAngles | Set the section angles for axis-symmetric model for which annotation is defined. |
SetSectors | Set the sector ids for cyclic-symmetric model for which annotation is defined |
SetUpdateEntityOnResultChange | Set weather entity is to be updated in case of result update for min/max annotation |
SetUsertext | Set the user text |
Enumerations¶
PostAnnotationBuilderType Enumeration | select option to define the annotation type |
Method Detail¶
CommitAnnotation¶
-
PostAnnotationBuilder.
CommitAnnotation
¶ Commits the annotation to create annotation object
Signature
CommitAnnotation()
Returns: Return type: NXOpen.CAE.PostAnnotation
New in version NX11.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
Delete¶
-
PostAnnotationBuilder.
Delete
¶ Deletes the annotation builder.
User must call
TransientObject.Dispose()
after calling this method.Signature
Delete()
New in version NX11.0.0.
License requirements: None.
Dispose¶
-
PostAnnotationBuilder.
Dispose
¶ Frees the object from memory.
After this method is called, it is illegal to use the object. In .NET, this method is automatically called when the object is deleted by the garbage collector.
Signature
Dispose()
New in version NX11.0.0.
License requirements: None.
SetAnnotationType¶
-
PostAnnotationBuilder.
SetAnnotationType
¶ Set the annotation type
Signature
SetAnnotationType(type)
Parameters: type ( NXOpen.CAE.PostAnnotationBuilderType
) –New in version NX11.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
SetCoordinate¶
-
PostAnnotationBuilder.
SetCoordinate
¶ Set the coordinates for user annotation
Signature
SetCoordinate(xcord, ycord)
Parameters: - xcord (float) –
- ycord (float) –
New in version NX11.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
SetEdgeFace¶
-
PostAnnotationBuilder.
SetEdgeFace
¶ Set the edge or face id for which annotation is defined
Signature
SetEdgeFace(subIds)
Parameters: subIds (list of int) – New in version NX11.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
SetElements¶
-
PostAnnotationBuilder.
SetElements
¶ Set the element ids for which annotation is defined
Signature
SetElements(elementIds)
Parameters: elementIds (list of int) – New in version NX11.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
SetName¶
-
PostAnnotationBuilder.
SetName
¶ Set the annotation name
Signature
SetName(name)
Parameters: name (str) – New in version NX11.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
SetNodes¶
-
PostAnnotationBuilder.
SetNodes
¶ Set the node ids for which annotation is defined
Signature
SetNodes(nodeIds)
Parameters: nodeIds (list of int) – New in version NX11.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
SetNumMinMax¶
-
PostAnnotationBuilder.
SetNumMinMax
¶ Set the number of min/max annotation for min/max type of annotation
Signature
SetNumMinMax(numMinMax)
Parameters: numMinMax (int) – New in version NX11.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
SetSectionAngles¶
-
PostAnnotationBuilder.
SetSectionAngles
¶ Set the section angles for axis-symmetric model for which annotation is defined.
The list of sections depend on current postview and how it is created using
NXOpen.CAE.AxiSymmetricParameters
Signature
SetSectionAngles(sectionAngles)
Parameters: sectionAngles (list of float) – New in version NX11.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
SetSectors¶
-
PostAnnotationBuilder.
SetSectors
¶ Set the sector ids for cyclic-symmetric model for which annotation is defined
Signature
SetSectors(sectorIds)
Parameters: sectorIds (list of int) – New in version NX11.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
SetUpdateEntityOnResultChange¶
-
PostAnnotationBuilder.
SetUpdateEntityOnResultChange
¶ Set weather entity is to be updated in case of result update for min/max annotation
Signature
SetUpdateEntityOnResultChange(update)
Parameters: update (bool) – New in version NX11.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)