ModelDisplayBuilderFreeEdgeMarker Enumeration¶
NXOpen.CAE.ModelDisplayBuilder.FreeEdgeMarker is an alias for NXOpen.CAE.ModelDisplayBuilderFreeEdgeMarker
-
class
NXOpen.CAE.
ModelDisplayBuilderFreeEdgeMarker
¶ Bases:
object
specifies the marker for endpoints of geometry free edges
New in version NX7.5.2.
Enum Members
Enum Member Enum Member Description NotSet No markerPlus Plus markerDot Dot markerAsterisk Asterisk markerCircle Circle markerPoundsign Pound sign markerCross Cross markerSquare Square markerTriangle Triangle markerDiamond Diamond markerCenterLine Center line marker-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-